Hi NXP.
I have a question about the i.MX6 solo's MAPSR register.
Looking at the register details in 45.12.17, the reset value of bit16 is 0.
Therefore, I think it is appropriate to set bit 16 to 0 when writing to the MAPSR register.
However, as shown below, in the document, 1 is set when writing to the MAPSR register.
In the Excel file, 1 is written as a fixed value to bit 16 of the MAPSR register.
Should bit16 be set to 1 when writing to the MAPSR register?
I would like to know the recommended value to write to bit16.
Best regards.
Solved! Go to Solution.
For the 19–16 This field is reserved. So for the bit 16 you can use the value in the
For the 19–16 This field is reserved. So for the bit 16 you can use the value in the