i.MX6qp initramfs bundled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6qp initramfs bundled

跳至解决方案
1,744 次查看
georgechiao
Contributor II

Hi,

I have searched a few days with no luck hence hoping someone could help if I post my issue instead.

I managed to build a bundled zImage-initramfs-xxx.bin which is just a 'core-image-minimal' for machine 'imx6qpsabresd'.  Note this is a bundled initramfs file which includes both kernel and initramfs.cpio.gz.  A few u-boot files (e.g. 'u-boot-xxx') and device tree files (e.g. xxx.dtb) were also being generated together with the bundled zImage-initramfs-xxxx.bin.

The frustrating bit is I have a imx6qp Sabre board right in front of me and I wasn't able to boot from the zImage-initramfs-xxx.bin.  BTW I did manage to flash the SD card with the '*.sdcard' image built previously and it worked fine but that has 'rootfs'.  I also tried to flash 'u-boot', 'device tree', 'zImage' and 'rootfs' to the SD card accordingly, and it worked as well; and I thought I could just flash 'zImage-initramfs-xxx.bin' instead of 'zImage' and 'rootfs' it should work but it didn't.   Messages below are from the console-

'switch to partitions #0. OK'

'mmc1 is current device'

'Unrecognized filesystem type'

...

'Bad Linux ARM zImage magic!'

Someone suggested me 'mfgtools v2' but unfortunately I hit a different issue, as for some reason my Win 7 had never shown the device as 'HID-Compliant Device', instead it was seen as 'USB Serial Port', which resulted in 'Unassigned' and 'No Device Connected' (see attached).

Any idea?  is it something to do with the u-boot file which I used is not for the bundled 'zImage-initramfs-xxx.bin'? or something I've done completely wrong?

Many thanks in advanced.

0 项奖励
1 解答
1,326 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

please look at initramfs usage on

i.MX6 Sabre SDB Booting from initramfs 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,327 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George

please look at initramfs usage on

i.MX6 Sabre SDB Booting from initramfs 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------