Hi,
I have a customized PCB which MCIMX6Y1 on board and choose ENET1 as the default ethernet port.
As I know the configuration in dts already declared two ethernet port via mdio bus.
But according to the log message, i.MX6ULL always setup ENET2 only.
I try to remove the configuration of ENET2 in dts, ethernet function still not functional.
Is there any way to setup the ENET1 correctly?
Thank you.
Hi Kyle
one can test if enet is working in uboot, check
#define CONFIG_FEC_ENET_DEV in uboot/include/configs/mx6ullevk.h
uboot-imx.git - Freescale i.MX u-boot Tree
also check clocks imx6ul_enet_clk_init() in linux/arch/arm/mach-imx/mach-imx6ul.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you. I will check it.