i.MX6ULL RM CSI interface shifted

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6ULL RM CSI interface shifted

跳至解决方案
1,616 次查看
chris321
Contributor IV

according to the i.MX6ULL reference manual (p 1666/4127 ... 1673) ALT0 for 

CSI_DATA00 is CSI_DATA02

CSI_DATA01 is CSI_DATA03

...

CSI_DATA07 is CSI_DATA09

thats somehow strange, shouldn't has ALT0 the same CSI data numbering as the pad name?

标签 (1)
标记 (2)
1 解答
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Chris,

i.M6ULL has only 289 ball pads, all functional signals can not be escaped out at the same time, they will be multiplexed in different group pins instead. For CSI module, only CSI_MCLK, CSI_PICCLK, CSI_VSYNC, CSI_HSYNC and CSI_DATA[07:00] ball pads are defined and escaped out. As described in 4.1.1 Muxing Options table, the ball pads CSI_DATA[07:00] are mapped to the internal CSI module functional signals CSI_DATA[9:2].

 

i.MX6ULL_CSI_MUX1.PNGi.MX6ULL_CSI_MUX2.PNGi.MX6ULL_CSI_MUX3.PNG

 

On our EVK board, it uses only 8-bit CSI data lines (CSI_DATA[07:00] -> CSI_DATA[9:2]). When  connect to an external 10-bit sensor, the least 2 bits are not used, and our SDK handles it in this way also. If customers want to use the full 10 bits or even more data bits, they can multiplex them to ball pads as 4.1.1 Muxing Options table.

 

The CSI module signal CSI_DATA0 can be multiplexed on ball pad LCD_DATA17 or UART3_RX_DATAbut not on ball pad of CSI_DATA00.

 

It is not so good to name the net name of CSI_DATA[07_00] ball pads connection as CSI_DATA[7:0] on the EVK schematic, but there is not typo in this RM section.

 

 

Best regards,

Carlos

在原帖中查看解决方案

9 回复数
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi chris321,

The RM description is correct. The CSI module can support 24-bit data with DATA[9:2] multiplexed to pads CSI_DATA[07:00], DATA1 multiplexed to  pad LCD_DATA16 and DATA0 multiplexed to LCD_DATA17. For more detail, please refer to the 4.1.1 Muxing Options Table. Thanks!

pastedImage_1.png


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
1,233 次查看
chris321
Contributor IV

Hi Carlos,

According to the table you copied from the RM the signal CSI_DATA0 is available at pin LCD_DATA17 (B13) but not available on CSI_DATA00 (E4).
Correct?

0 项奖励
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi chris,

that is correct.

0 项奖励
1,233 次查看
chris321
Contributor IV

Ok thank you for your time.

But I just found that in the reference schematic SPF-29364_a the signal CSI_DATA0 is connected to pin CSI_DATA00. That conflicts somehow with the above.

0 项奖励
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Let me check.

0 项奖励
1,234 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Chris,

i.M6ULL has only 289 ball pads, all functional signals can not be escaped out at the same time, they will be multiplexed in different group pins instead. For CSI module, only CSI_MCLK, CSI_PICCLK, CSI_VSYNC, CSI_HSYNC and CSI_DATA[07:00] ball pads are defined and escaped out. As described in 4.1.1 Muxing Options table, the ball pads CSI_DATA[07:00] are mapped to the internal CSI module functional signals CSI_DATA[9:2].

 

i.MX6ULL_CSI_MUX1.PNGi.MX6ULL_CSI_MUX2.PNGi.MX6ULL_CSI_MUX3.PNG

 

On our EVK board, it uses only 8-bit CSI data lines (CSI_DATA[07:00] -> CSI_DATA[9:2]). When  connect to an external 10-bit sensor, the least 2 bits are not used, and our SDK handles it in this way also. If customers want to use the full 10 bits or even more data bits, they can multiplex them to ball pads as 4.1.1 Muxing Options table.

 

The CSI module signal CSI_DATA0 can be multiplexed on ball pad LCD_DATA17 or UART3_RX_DATAbut not on ball pad of CSI_DATA00.

 

It is not so good to name the net name of CSI_DATA[07_00] ball pads connection as CSI_DATA[7:0] on the EVK schematic, but there is not typo in this RM section.

 

 

Best regards,

Carlos

1,233 次查看
chris321
Contributor IV

Hi Carlos,

I am aware that ALT0 doesn't has to be the main function and thus the pin name.

CSI_DATA00 function is not available on CSI_DATA00 pin according to the MUX table, that's whats confusing me.

0 项奖励
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Ok ok, now I goy you.

Let me check, sounds like a typo.

Thanks Carlos

0 项奖励
1,233 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi chris321,

As you may know each pin on i.MX devices has up to 8 potential functions, and on the other side, one function can be available in different pins.

One of the 8 functions is chosen as the "main" function and this is how the pin will be named, but it is not necessary to be ALT 0, it could be any.

Regards,

Carlos

0 项奖励