i.MX6ULL LCD Connections

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL LCD Connections

837件の閲覧回数
daneduplooy
Contributor III

Hi! I am brand new to application processors and am busy designing our first board. I have a few questions regarding the LCD interface please:

1. What is the mapping for the LCD_DATA00 - LCD_DATA23 signals to R0-R7 / G0-G7 / B0-B7?

2. Does "LCD_ENABLE" correlate to "DE" on the TFT?

3. Does "LCD_RESET" correlate to "DISP" on the TFT?

This would be for connecting a display like 4DLCD-43480272

https://4dsystems.com.au/catalog/product/view/id/955/s/4dlcd-43480272-ips/

https://4dsystems.com.au/mwdownloads/download/link/id/824/

Thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

778件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For the RGB connection please see this:

6ULL LCD RGB.PNG

For the LCD_ENABLE and LCD_RESET please see our reference design.

The default supported LCD is the LCD8000-43T, it is the validated module, which has a 4.3 inch resistive touch screen and supports a resolution of up to 480x3(RGB)x272.

Hope this can do help for you

 

0 件の賞賛
返信