Hi,
I'm currently trying to boot via eMMC connected to usdhc2
on a custom i.MX6UL board. The device is working correctly. I've
testing this by loading U-Boot via USB or JTAG. But I've been
trying very hard to get booting from this eMMC to work. Without
success so far. And now my best guess is, that the pin-muxing
for this device on this custom board is not supported (incompatible)
by the BootROM. Here how its connected:
static iomux_v3_cfg_t const usdhc2_pads[] = {
MX6_PAD_CSI_VSYNC__USDHC2_CLK | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_CSI_HSYNC__USDHC2_CMD | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA00__USDHC2_DATA0 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA01__USDHC2_DATA1 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA02__USDHC2_DATA2 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA03__USDHC2_DATA3 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA04__USDHC2_DATA4 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA05__USDHC2_DATA5 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA06__USDHC2_DATA6 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
MX6_PAD_NAND_DATA07__USDHC2_DATA7 | MUX_PAD_CTRL(USDHC_PAD_CTRL),
/*
* RST_B
*/
MX6_PAD_GPIO1_IO09__USDHC2_RESET_B | MUX_PAD_CTRL(NO_PAD_CTRL),
};
As you see, this differs at least in the CLK and CMD pins from
your i.MX6UL eval board. And the manual even lists in chapter
"8.5.3.4 IOMUX Configuration for SD/MMC" the supported pins.
This also suggests that the current pin configuration is not
supported and can't boot at all.
Before we do a redesign of this board, could you please comment
on this? Are my findings correct here? Is there some other
possibility to get the BootROM to use our pin-muxing for this
USDHC2 interface?
Any insights here are really appreciated.
Thanks,
Stefan
已解决! 转到解答。
Hi Stefan
BootROM can not boot with these settings as it
uses hardware fixed pin-muxing as described in RM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Stefan
BootROM can not boot with these settings as it
uses hardware fixed pin-muxing as described in RM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------