i.MX6UL and PMIC power connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL and PMIC power connections

1,229 次查看
surendrajadhav
Contributor IV

Hi,

 

i.MX6UL has VDD_SoC_IN and VDD_ARM_CAP power rails to drive internal core and other logic circuit. Its operating range is from 0.925V to 1.3V(Max. and LDO bypassed).The same is shown in attached image as CPU_Power.

While PMIC IC(MC34PF3000A7EP) we used preprogrammed OTP configuration with which default supply available on OTP_SW1B_VOT rail is 1.4V as shown attached images PMIC_PWR1 and PMIC_PWR2. We have connected this PMIC rails to VDD_SoC _IN and VDD_ARM_CAP. The same observed in one of the Evaluation kit.

I am worried as PMIC output is exceeding the required CPU input voltage.

 

Let me know your inputs on this.

 

Regards,

Surendra Jadhav.

标签 (2)
0 项奖励
1 回复

910 次查看
Yuri
NXP Employee
NXP Employee

Hello

  Please refer to https://community.nxp.com/message/864046 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励