Hi,
i.MX6UL has VDD_SoC_IN and VDD_ARM_CAP power rails to drive internal core and other logic circuit. Its operating range is from 0.925V to 1.3V(Max. and LDO bypassed).The same is shown in attached image as CPU_Power.
While PMIC IC(MC34PF3000A7EP) we used preprogrammed OTP configuration with which default supply available on OTP_SW1B_VOT rail is 1.4V as shown attached images PMIC_PWR1 and PMIC_PWR2. We have connected this PMIC rails to VDD_SoC _IN and VDD_ARM_CAP. The same observed in one of the Evaluation kit.
I am worried as PMIC output is exceeding the required CPU input voltage.
Let me know your inputs on this.
Regards,
Surendra Jadhav.
Hi Surendra
by default processor works in ldo enabled mode, with max.1.5V according to
Table 11 Operating Ranges Datasheet http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf
Immediately after power up, software can change pmic voltages if necessary .
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------