i.MX6UL USB OTG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6UL USB OTG

916 次查看
martinwerner
Contributor I

I have a question regarding the USB OTG interface on the IMX6UL. I am using the i.MX6UL in a custom Hardware Design and I am wondering if it is neccessary to set the ID Signal High or Low by external Components. I need a lot of Interfaces and Analog Inputs, so the muxed Pins ID, OC and PWR are blocked by other functions.

Is it possible to set these by Software?

Best regards

Martin

标签 (1)
标记 (1)
0 项奖励
2 回复数

583 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Martin

per usb specification ID signal should be high (or float) in Device mode,

low in Host. It is used by linux driver,  I am afraid it is not possible to set it by software

without additional modifications in linux sources.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

583 次查看
martinwerner
Contributor I

BTW: I want to use the i.MX6 as USB Host.

0 项奖励