i.MX6UL EVK with Murata ZP integration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6UL EVK with Murata ZP integration

636 Views
soumyaks
Contributor II

Hi,

I am using Murata ZP BCM4339 module with i.MX6ULEVK kit. The BCM driver is provided along with the Linux 4.1.15 that i am using. 

I have used the Murata Users Guide and got the BCM module up and running on the image provided by them which is Linux version 3.14.

But on the Linux 4.1.15, i get the following error when I modprobe the driver.  

root@imx6ulevk:~# ifconfig wlan0 up
Dongle Host Driver, version 1.141.92 (r)
Compiled in drivers/net/wireless/bcmdhd
wl_android_wifi_on in
mmc0: queuing unknown CIS tuple 0x80 (2 bytes)
mmc0: queuing unknown CIS tuple 0x80 (7 bytes)
mmc0: queuing unknown CIS tuple 0x80 (6 bytes)
F1 signature OK, socitype:0x1 chip:0x4339 rev:0x1 pkg:0x0
DHD: dongle ram size is set to 786432(orig 786432) at 0x180000
_dhdsdio_download_firmware: dongle image file download failed
dhd_net_bus_devreset: dhd_bus_devreset: -35
dhd_open : wl_android_wifi_on failed (-35)
wl_android_wifi_off in
dhd_prot_ioctl : bus is down. we have nothing to do
dhd_net_bus_devreset: dhd_bus_devreset: -35
ifconfig: SIOCSIFFLAGS: Operation not permitted
The BUS down error is seen even when I take the BCMDHD firmware images from the 3.14 and load it in 4.1.15.
My dts looks like this:
&iomuxc {
imx6ul-evk-murata-v2 {
pinctrl_wifi: wifigrp {
fsl,pins = <
MX6UL_PAD_SNVS_TAMPER1__GPIO5_IO01 0x03029
>;
};
};
Can anyone please tell where I might be going wrong?
Many Thanks in advance,
Soumya 
0 Kudos
1 Reply

394 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Soumya,

   According to your logs, before loading dhd.ko, firmware files were not loaded correctly, so you can use insmod command to load driver module with parameters, like bellow:

# insmod /system/lib/dhd.ko "firmware_path=/system/etc/sdio-g-cdc-full11n-reclaim-roml-wme-idsup.bin nvram_path=/system/etc/nvram.txt"

   you can ajust your firmware path according to your system.


Have a great day,
(weidong)

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos