imx6 - 20-bit parallel camera with 1080@60fps

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 - 20-bit parallel camera with 1080@60fps

994 次查看
Ansari
Contributor IV

Dear support team,

We are using imx6Q custom platform based on sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.
 
We would like to use a 20-bit parallel camera input through CSI0. 

Please let us know, will the CSI0 support 1920x1080P @60fps?

Thanks and Regards,

Ansari

0 项奖励
回复
1 回复

796 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ansari

yes it supports, CSI IPU performance is described in sect.37.1.2.1.1 Camera Ports i.MX6DQ RM

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf 

For parallel interface, the maximum speed of the interface is 240Mhz.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复