Hi,
I am using Murata ZP BCM4339 module with i.MX6ULEVK kit. The BCM driver is provided along with the Linux 4.1.15 that i am using.
I have used the Murata Users Guide and got the BCM module up and running on the image provided by them which is Linux version 3.14.
But on the Linux 4.1.15, i get the following error when I modprobe the driver.
Hello Soumya,
According to your logs, before loading dhd.ko, firmware files were not loaded correctly, so you can use insmod command to load driver module with parameters, like bellow:
# insmod /system/lib/dhd.ko "firmware_path=/system/etc/sdio-g-cdc-full11n-reclaim-roml-wme-idsup.bin nvram_path=/system/etc/nvram.txt"
you can ajust your firmware path according to your system.
Have a great day,
(weidong)
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------