When I read the reference manual ( Document Number: IMX6ULRM
Rev. 2, 03/2017 ) page 614/3619, there is a divider in the clock tree for the QSPI1_CLK_ROOT that could be used (CSCMR1[QSPI1_PODF] ).
The divider QSPI_PODF could only divide by 1, 2 or 8.
Could we use other dividers such as 3, 4 , 5, or 6 or is it a mistake in the reference manual ?
I have a doubt about that because I downloaded the NXP SDK ( Release Name: MCUXpresso Software Development Kit (SDK)
Release Version: 2.2.0 ) and in nearly all example provided for the evkimx6ul board, the value of 5(divide by 6) is used.
You can check the following file from the SDK for example
./boards/evkmcimx6ul/rtos_examples/freertos_hello/clock_config_ocram.c:
CCM->CSCMR1 = (CCM->CSCMR1 & ~(CCM_CSCMR1_QSPI1_CLK_SEL_MASK | CCM_CSCMR1_QSPI1_PODF_MASK)) | CCM_CSCMR1_QSPI1_CLK_SEL(0) | CCM_CSCMR1_QSPI1_PODF(5);
已解决! 转到解答。
Hi @louneschibi
I hope you are doing well.
I have discussed this query with the internal team and concluded like it is printing mistake of Reference manual. One can set the QSPI_PODF from 1 to 8.
Thanks & Regards
Sanket Parekh
Hi @louneschibi
Yes, I will raise the request for the same with the help of NXP engineering team.
Thanks & Regards
Sanket Parekh
Hi @louneschibi
I hope you are doing well.
I have discussed this query with the internal team and concluded like it is printing mistake of Reference manual. One can set the QSPI_PODF from 1 to 8.
Thanks & Regards
Sanket Parekh