i.MX6SoloX video flickers upon PCIe access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SoloX video flickers upon PCIe access

477 Views
aivchenko
Contributor II

I'm debugging an SBC with i.MX6SoloX MCU on it. There is video output using LVDS lines and NVME drive on PCIe.

When I copy significant files over PCIe into NVME LVDS output flickers (the video page is static at this time).

Running Yocto/Rocko

What should I look for? Could it be an issue with Linux BSP or this is more of a signal interference issue in hardware?

Does video output depends on the load of the CPU core or DMA?

Labels (1)
0 Kudos
1 Reply

405 Views
art
NXP Employee
NXP Employee

The most likely cause of the issue is the memory bus bandwidth limitation that causes the video output breach during an intense data transfer. The possible solution is the memory usage optimization, transferring data by a smaller portions etc.


Have a great day,
Artur

0 Kudos