Hi,
I have both i.MX6Q and i.MX6SoloX based HW.
They are running image built from same sources in Yocto (except of course device tree etc.. differences).
I noticed that if I run weston-smoke app in i.MX6Q based hw (with 1024x768 resolution although actual app is smaller) the CPU usage is around 22%. If I run the same app in i.MX6SoloX based hw (with 320x340 resolution and app is smaller) the CPU usage is around 87%.
I was wondering could it be because the i.MX6SoloX based hw prints this at bootup:
galcore: clk_get 2d core clock failed, disable 2d/vg
Galcore version: 5.0.11.41671
I looked at the Linux other i.MX6SoloX device configs and couldn't find that any of them configured the 2d clock like it's done in i.MX6Q. i.MX6SoloX should have 2D/VG acceleration if I've understood right, but why it's not used in Linux? Or am I completely mistaken here?
解決済! 解決策の投稿を見る。
Hi mc
you are right i.MX6SoloX has 2D/VG acceleration, however compared
with i.MX6Q there is only one gpu (GC400), i.MX6Q has dedicated 2D gpu module.
One can find gpus description on p.5,6
http://cache.freescale.com/files/training/doc/dwf/DWF13_AMF_CON_T1025.pdf
Seems linux uses 3D, so 2D can not be used as they share same logic, please
look at Figure 33-1. GPU Block Diagram i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi mc
you are right i.MX6SoloX has 2D/VG acceleration, however compared
with i.MX6Q there is only one gpu (GC400), i.MX6Q has dedicated 2D gpu module.
One can find gpus description on p.5,6
http://cache.freescale.com/files/training/doc/dwf/DWF13_AMF_CON_T1025.pdf
Seems linux uses 3D, so 2D can not be used as they share same logic, please
look at Figure 33-1. GPU Block Diagram i.MX6SX Reference Manual
http://www.nxp.com/docs/en/reference-manual/IMX6SXRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks, that makes sense then that 2D is slower since the 3D accelerated instead. I didn't pick that when I looked through the documentation.