Hi All,
We're migrating our Android 4.2 platform from an iMX6Solo design to an iMXSoloLite design, and we're experiencing a hang while flushing the TLBs (local_flush_tlb_all) during Linux (mfg-tool configured) boot.
Specifics:
The hang occurs while the mfg tool version of the kernel is booting: devicemaps_init() --> local_flush_tlb_all() --> invalidate all TLBs.
Any help in understanding or troubleshooting this problem would be greatly appreciated.
Cheers,
-John
So. here is working config for 3.0.35
https://yadi.sk/d/W5YMECttg2cdY
Default configs for imx6sl are not working for me.
Thank you for the reply. I have resolved this issue. I have a new problem! During boot, the CPU is stuck in an infinite loop waiting for the GPU to complete its reset -- it's stuck in _ResetGPU. I've validated that the LDOs are setup properly (we're using internal LDOs). Any pointers to solve this issue would be greatly appreciated.
It's an im6sl design using the jb4.3_1.1.0-ga version of the kernel.
Thanks,
-John
Hello John Kaye,
Nice to hear that you resolved the TBL flush issue. We are migrating from 3.0.35 Linux to 3.11 linux are during bootup it hangs in devicemaps_init() --> local_flush_tlb_all() --> invalidate all TLBs.
Please suggest us the solution which helped you to solve this problem.
Thank you
Regards,
Sanju.