I have ported over the i.MX6UL FreeRTOS SDMA and sdma_memory_to_memory example application to the i.MX6SX platform for the Cortex-M4 core. When I run the application I get some strange behavior dependent upon the "count" parameter of the SDMA BD.
Platform: i.MX6SX SABRE-SDB
Software: FreeRTOS_BSP_1.0.1_iMX6SX
Toolchain: GNU Tools for Arm Embedded Processors 7-2018-q3-update
Expected Behavior:
* All bytes in the source buffer are correctly copied to the destination buffer via the SDMA
Actual Behavior:
* For counts 1-7, the source is correctly copied to the destination buffer.
* For count of 8 bytes, the first 4 bytes of the source are copied to the destination, then the next 4 bytes are copied to offset 12 (incorrectly skipping 8 bytes).
* For a count of 12 bytes, the behavior of 8 bytes is observed, but then the source bytes at offsets 8-11 are correctly located at destination offsets 8-11.
* For a count of 16 bytes, the behavior of 12 bytes is observed, but bytes at source offsets 8-15 are reproduced at destination offsets 16-23. This means bytes at offsets 8-11 are duplicated.
Steps to Reproduce:
1. Download the attached memory_to_memory.zip example
2. Create the directory FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/driver_examples/sdma
3. Extract the zip file to the location FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/driver_examples/sdma. A directory containing source should be created at FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/driver_examples/sdma/memory_to_memory.
4. Build with the script build_debug.sh in the FreeRTOS_BSP_1.0.1_iMX6SX/examples/imx6sx_sdb_m4/driver_examples/sdma/memory_to_memory/armgcc.
5. Load and run the resulting binary within u-boot.
Notes:
* All memory is within the TCM so as to eliminate external memory configuration concerns.
Is there some misconfiguration within my program that would cause the SDMA M2M (IMX6SXRM Appendix A ap_2_ap) script to perform this behavior?
Thanks,
Jake
2018-10-30: The requested file has been uploaded.
Regards,
Jake
解決済! 解決策の投稿を見る。
Hi Jacob,
I think the problem is that the SDMA scripts are made from the Cortex-A perspective, the iMX6UL has only a Cortex-A9 core so that's why it has a SDMA M2M example. You would need to modify the SDMA scripts to make them work with the M4 core.
Unfortunately we cannot provide the SDMA scripts source code and/or modifications, this is out of the standard support that we provide. You can contact Professional Services to check if this is something that can be done.
Reference: https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE
Contact: Prosupport@nxp.com
Thanks!
Vanessa
Could you please send me the full project folder with your modifications (FreeRTOS_BSP_1.0.1_iMX6SX)?
I see some missing files trying to compile just by adding the "memory_to_memory" folder.
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/drivers/src/ccm_analog_imx6sx.c:31:31: fatal error: ccm_analog_imx6sx.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/drivers/src/ccm_imx6sx.c:31:24: fatal error: ccm_imx6sx.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/utilities/src/debug_console_imx.c:35:24: fatal error: device_imx.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/drivers/src/lmem.c:31:18: fatal error: lmem.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/drivers/src/ccm_analog_imx6sx.c:31:31: fatal error: ccm_analog_imx6sx.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/drivers/src/ccm_imx6sx.c:31:24: fatal error: ccm_imx6sx.h: No such file or directory
/home/vanessa/Documents/community/487273_sx_sdma_m2m/FreeRTOS_BSP_1.0.1_iMX6SX/platform/utilities/src/debug_console_imx.c:35:24: fatal error: device_imx.h: No such file or directory
I could copy the files from the 6UL SDK but I just want to make sure I have the same setup as yours.
Thanks in advance!
Best Regards,
Vanessa
Hi Vanessa,
I have uploaded the complete project folder as FreeRTOS_BSP_1.0.1_iMX6SX_SDMA.tgz.
Regards,
Jake
Hi Jacob,
I received your package and I can see the issue on my board.
I started investigating this and I'll probably have an answer by next week (will be out of office tomorrow).
Thanks!
Vanessa
vanessamaegima, can you help with this thread?
Sure Karina, I will investigate this.