I recently purchased an i.MX6 Sololite EVK (MCIMX6SLEVK Rev B1) for a project I'm working on, and would like to 3D print a case for it.
I've had a look through the design files download, including the schematics and layout directories, but I can't see anything that shows the physical layout and dimensions. Ideally it would include positions of the various ports such as power, USB, SD cards, etc. Does anything like that exist?
已解决! 转到解答。
Hello Rebecca,
In the Design Files of the EVK, there is the Power, USB and SDcard as well in the layout file is the physical dimension of the board, maybe i miss something here.
regards