i.MX6SL EVK board dimensions & physical layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SL EVK board dimensions & physical layout

Jump to solution
727 Views
bexc
Contributor I

I recently purchased an i.MX6 Sololite EVK (MCIMX6SLEVK Rev B1) for a project I'm working on, and would like to 3D print a case for it.

I've had a look through the design files download, including the schematics and layout directories, but I can't see anything that shows the physical layout and dimensions. Ideally it would include positions of the various ports such as power, USB, SD cards, etc. Does anything like that exist?

Labels (1)
1 Solution
635 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Rebecca,

In the Design Files of the EVK, there is the Power, USB and SDcard as well in the layout file is the physical dimension of the board, maybe i miss something here.

regards

View solution in original post

2 Replies
636 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Rebecca,

In the Design Files of the EVK, there is the Power, USB and SDcard as well in the layout file is the physical dimension of the board, maybe i miss something here.

regards

635 Views
bexc
Contributor I

I had to do some research to find the free Cadence Allegro Physical Viewer, but once I installed it I was able to see the board in the .brd file. Thanks!