Hi,
I would like some input on troubleshooting a NOR flash on an i.MX6.
It is a custom board
CPU: i.MX6
Flash: Spansion S29GL256S90TFI010
Boot config: NOR Flash
SRC_SBMR1 = 0x26004000 , Not multiplexed 01 - A+DH, NOR flash
BOOT_MODE[1:0] = 10
BOOT_FUSE_SEL = 0
It is connected similar to the SABRE AI,
Issues:
I can't access it and since I can't access it it's obviously empty and the internal boot hangs trying the backup boot via serial USB.
I've tried to access the flash via Lauterbach and J-link. No luck
I've copied the EIM and CCM registers from the internal BOOT settings to use with the T32 imx6 sample script, I've converted it to i.MX6S from i.MX6Q.
When running the T32 flash script it stops on the first Flash access. (attached is T32 flash cmm)
Any ideas?
Of course it can be Hw related but I'd like any input for possible Sw issues in parallel.
Regards
Andreas
Original Attachment has been moved to: imx6s-norflash.cmm.txt.zip
Hi andreas
one can check NOR with SDK (one can run it with jtag) eim_test.c
i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I did and it end up in an exception in the beginning of the code of flash_get_size.
Am I correct if I assume that the internal boot will setup the EIM bus correct if the boot_cfg is correct?
Not optimal but working. Based on that assumption I've commented out the "eim_hw_prepare" since I have a different flash, at first glance it looks like I could re-use.