i.MX6S LVDS min frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6S LVDS min frequency

614 Views
darrellblock
NXP Employee
NXP Employee

Customer is using LVDS channel 1 only and connecting this LVDS directly to 10.1” display via LVDS, and, on another application, connecting it to 4.3” via an LVDS to RGB converter.  The 4.3” display is an RGB display and requires its DOTCLK frequency to be at 8.54MHz.

 

The question is, can the IMX LVDS controller frequency to be set as low as 8.54MHz?

 

 

pastedImage_1.png

Labels (1)
0 Kudos
Reply
1 Reply

495 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Darrell Block,

I’m afraid 8.54 MHz would not be achievable. This is a very rare LVDS frequency and the achievable frequencies for the Display Interface Clock start at 20Mhz but I haven’t seen any actual application below around 30Mhz.

Regards,

0 Kudos
Reply