i.MX6Quad RTC typical power consumption in SNVS mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Quad RTC typical power consumption in SNVS mode

ソリューションへジャンプ
1,012件の閲覧回数
RussellPead
Contributor II
  1. For the i.MX6Quad, is the 4uA typical for an external crystal for the RTC (Table 19 page 35) included in the 41uA typical in SNVS mode (Table 9 page 25) or is it separate with total current 45uA typical?


Referenced Document Number: IMX6DQIEC     i.MX6D/Q Datasheet

Rev. 3, 03/2014

0 件の賞賛
1 解決策
720件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
721件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
720件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Russell

yes this data is included in 41uA typical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛