i.MX6Q uSDHC UHS support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6Q uSDHC UHS support

1,246 次查看
NithinkumarN
Contributor II

Hi all,

I'm using i.MX6Q L3.0.35_4.1.0 freescale release in my project.

I need to test UHS-1 Micro SD card in my custom board.

Please let me know is this code release supports this feature?

If not what changes to be done in code as well as board to support this feature.

Thanks and Regards,

Nithin

标签 (2)
0 项奖励
回复
4 回复数

1,013 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nithin

I am afraid this release does not support UHS, suggest to try

latest BSP:

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,013 次查看
NithinkumarN
Contributor II

Hi Igor,

I need to test UHS-1 DDR50 mode in my board.

Is this support also not present in Linux 3.0.35 kernel of L3.0.35_4.1.0 release?

Thanks and Regards,

Nithin

0 项奖励
回复

1,013 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nithin

I am afraid not. However it works in latest releases.

Best regards

igor

1,013 次查看
NithinkumarN
Contributor II

Hi Igor,

Is there any patch file present for Linux 3.0.35 to support UHS-1 in it.

Thanks and Regards,

Nithin

0 项奖励
回复