i.MX6Q eMMC boot issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q eMMC boot issue

Jump to solution
7,667 Views
jasonhsu
Contributor III

Hi, All

We designed a customer board based on imx6q SabreAI board, and use SD3 as eMMC boot.

Now, it can download firmware with MFG Tool, however, it cannot boot up, because the board is always in download mode ( MFGTool always display " HID-compliance device".)

Maybe there are some mistakes when partitionion or MBR in the 1st 1kb of eMMC, but i'm not sure.

Could some one give some suggestion to help me to go forward.

below is the log of download using mfg tool.

=============================

U-Boot 2009.08-svn30 (May 24 2014 - 12:29:00)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 183

Temperature:   31 C, calibration data 0x5874d47d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock     : 528000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6Q-SABREAUTO: unknown-board Board: 0x63012 [POR]

Boot Device: MMC

I2C:   ready

DRAM:   2 GB

MMC:   mmc init ok - jason

FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

Using default environment

In:    serial

Out:   serial

Err:   serial

Found PFUZE100! deviceid=10,revid=11

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35-svn27

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3183872 Bytes =  3 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 10c00000 ...

   Image Name:   uboot initramfs rootfs

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    4545326 Bytes =  4.3 MB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Linux version 3.0.35-svn27 (xujianhua@semisky3) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #2 SMP PREEMPT Fri May 23 16:53:24 CST 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre Auto Board, Semisky Inc.

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @82063000 s5184 r8192 d15296 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 520192

Kernel command line: console=ttymxc1,115200 rdinit=/linuxrc enable_wait_mode=off

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)

Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)

Memory: 2048MB = 2048MB total

Memory: 2068248k/2068248k available, 28904k reserved, 360448K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xea800000 - 0xf2000000   ( 120 MB)

    lowmem  : 0x80000000 - 0xea000000   (1696 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x8003a000   ( 200 kB)

      .text : 0x8003a000 - 0x805b66f0   (5618 kB)

      .data : 0x805b8000 - 0x806064a0   ( 314 kB)

       .bss : 0x806064c4 - 0x806318f0   ( 174 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x21e8000 (options '115200')

bootconsole [ttymxc1] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

==<backlignt : 1 >n

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1048576 B

bio: create slab <bio-0> at 0

mxs-dma mxs-dma-apbh: initialized

print_constraints: VA: 2800 mV

print_constraints: VD: 2800 mV

print_constraints: VLS: 2800 mV

print_constraints: VLC: 2800 mV

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1

mc_pfuze 1-0008: FAB: 0 ,FIN: 0

print_constraints: SW1A: 300 <--> 1875 mV at 1375 mV

print_constraints: SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: SW1C: 300 <--> 1875 mV at 1375 mV

print_constraints: SW2: 800 <--> 3950 mV at 3000 mV

print_constraints: SW3A: 400 <--> 1975 mV at 1500 mV

print_constraints: SW3B: 400 <--> 1975 mV at 1500 mV

print_constraints: SW4: 800 <--> 3950 mV at 3300 mV

print_constraints: SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: VSNVS: 1200 <--> 3000 mV at 1800 mV

print_constraints: VREFDDR: at 750 mV

print_constraints: VGEN1: 800 <--> 1550 mV at 800 mV

print_constraints: VGEN2: 800 <--> 1550 mV at 1500 mV

print_constraints: VGEN3: 1800 <--> 3300 mV at 2800 mV

print_constraints: VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: VGEN5: 1800 <--> 3300 mV at 3000 mV

print_constraints: VGEN6: 1800 <--> 3300 mV at 2800 mV

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

Clockevents: could not switch to one-shot mode:

Clockevents: could not switch to one-shot mode:

Clockevents: could not switch to one-shot mode: dummy_timer is not functional.

dummy_timer is not functional.

Could not switch to high resolution mode on CPU 2

Clockevents: could not switch to one-shot mode:

Could not switch to high resolution mode on CPU 1

dummy_timer is not functional.

Could not switch to high resolution mode on CPU 0

NET: Registered protocol family 2

IP route cache hash table entries: 65536 (order: 6, 262144 bytes)

TCP established hash table entries: 262144 (order: 9, 2097152 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 262144 bind 65536)

TCP reno registered

UDP hash table entries: 1024 (order: 3, 32768 bytes)

UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Unpacking initramfs...

dummy_timer is not functional.

Could not switch to high resolution mode on CPU 3

Freeing initrd memory: 4436K

Static Power Management for Freescale i.MX6

wait mode is disabled for i.MX6

cpaddr = ea880000 suspend_iram_base=ea8e8000

PM driver module loaded

IMX usb wakeup probe

cpu regulator mode:ldo_enable

i.MXC CPU frequency driver

highmem bounce pool size: 64 pages

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

msgmni has been set to 3344

cryptodev: driver loaded.

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x37

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

console [ttymxc1] enabled, bootconsole disabled

console [ttymxc1] enabled, bootconsole disabled

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

loop: module loaded

GPMI NAND driver registered. (IMX)

vcan: Virtual CAN interface driver

FEC Ethernet Driver

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

add wake up source irq 75

g_file_storage gadget: controller 'fsl-usb2-udc' not recognized

check_parameters:UTP settings are in place now, overriding defaults

g_file_storage gadget: No serial-number string provided!

g_file_storage gadget: File-backed Storage Gadget, version: 1 September 2010

g_file_storage gadget: Number of LUNs=1

fsl-usb2-udc: bind to driver g_file_storage

mousedev: PS/2 mouse device common for all mice

=======================goodix_ts_init======================

============================goodix_ts_probe==========================

input: Goodix_TouchScreen_GT80X as /devices/virtual/input/input0

================goodix_init_panel===================

================goodix_init_panel===================

Goodix-TS 1-0055:  Guitar Version: GT801_1R08_2011121501_Goodix_Tech    

============== Guitar Version: GT801_1R08_2011121501_Goodix_Tech      ===============

g_file_storage gadget: high speed config #1

Goodix-TS 1-0055: Start  Goodix_TouchScreen_GT80X in Interrupt mode

i2c-core: driver [Goodix-TS] using legacy suspend method

i2c-core: driver [Goodix-TS] using legacy resume method

using rtc device, snvs_rtc, for alarms

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

sdhci sdhci-esdhc-imx.3: no card-detect pin available!

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA

sdhci sdhci-esdhc-imx.0: no write-protect pin available!

sdhci sdhci-esdhc-imx.0: no card-detect pin available!

mmc2: no vmmc regulator found

mmc2: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

Cirrus Logic CS42888 ALSA SoC Codec Driver

Device with ID register fffffffb is not a CS42888

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

imx_3stack asoc driver

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 008GE0 7.28 GiB

regulator_init_complete: VGEN6: incomplete constraints, leaving on

mmcblk0boot0: mmc0:0001 008GE0 partition 1 4.00 MiB

mmcblk0boot1: mmc0:0001 008GE0 partition 2 4.00 MiB

regulator_init_complete: VGEN5: incomplete constraints, leaving on

regulator_init_complete: VGEN4: incomplete constraints, leaving on

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

regulator_init_complete: VGEN2: incomplete constraints, leaving on

regulator_init_complete: VLC: incomplete constraints, leaving on

regulator_init_complete: VLS: incomplete constraints, leaving on

regulator_init_complete: VD: incomplete constraints, leaving on

regulator_init_complete: VA: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

mmcblk0: p4 size 13090816 extends beyond EOD, truncated

Freeing init memory: 200K

mmcblk0boot1: unknown partition table

Starting UTP

mmcblk0boot0: unknown partition table

ln: /etc/mtab: File exists

disable turn off display

Starting the hotplug events dispatcher udevd

udevd (2001): /proc/2001/oom_adj is deprecated, please use /proc/2001/oom_score_adj instead.

Synthesizing initial hotplug events

uuc 0.4 [built Aug 16 2013 01:24:08]

UTP: Waiting for device to appear

UTP: file/device node /dev/utp already exists

cpu_id is 0

UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16'

UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16"

16+0 records in

16+0 records out

8192 bytes (8.0KB) copied, 0.002714 seconds, 2.9MB/s

UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16.

utp_poll: pass returned.

UTP: received command '$ echo 0 > /sys/block/mmcblk0boot0/force_ro'

UTP: executing "echo 0 > /sys/block/mmcblk0boot0/force_ro"

UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk0boot0/force_ro.

utp_poll: pass returned.

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2'

UTP: executing "dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2"

910+1 records in

910+1 records out

466180 bytes (455.3KB) copied, 0.070847 seconds, 6.3MB/s

UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2.

utp_poll: pass returned.

UTP: received command '$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config'

UTP: executing "echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config"

UTP: sending Success to kernel for command $ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/mmc0:0001/boot_config.

utp_poll: pass returned.

UTP: received command '$ echo 1 > /sys/block/mmcblk0boot0/force_ro'

UTP: executing "echo 1 > /sys/block/mmcblk0boot0/force_ro"

UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk0boot0/force_ro.

utp_poll: pass returned.

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ tar xf $FILE '

UTP: executing "tar xf $FILE "

UTP: sending Success to kernel for command $ tar xf $FILE .

utp_poll: pass returned.

UTP: received command '$ sh -x mksdcard-android.sh /dev/mmcblk0'

UTP: executing "sh -x mksdcard-android.sh /dev/mmcblk0"

+ BOOTLOAD_RESERVE=8

+ BOOT_ROM_SIZE=8

+ SYSTEM_ROM_SIZE=512

+ CACHE_SIZE=512

+ RECOVERY_ROM_SIZE=8

+ VENDER_SIZE=8

+ MISC_SIZE=8

+ id -u

+ userid=0

+ [ 0 -ne 0 ]

+ moreoptions=1

+ node=na

+ cal_only=0

+ flash_images=0

+ not_partition=0

+ not_format_fs=0

+ [ 1 = 1 -a 1 -gt 0 ]

+ moreoptions=0

+ node=/dev/mmcblk0

+ [ 0 = 0 ]

+ [ 1 -gt 1 ]

+ [ 0 = 1 ]

+ [ 0 = 1 -a 1 - mmcblk0: unknown partition table

gt 0 ]

+ [ ! -e /dev/mmcblk0 ]

+ seprate=40

+ sfdisk -s /dev/mmcblk0

+ total_size=7634944

+ expr 7634944 / 1024

+ total_size=7456

+ expr 8 + 8

+ boot_rom_sizeb=16

+ expr 512 + 512 + 8 + 8 + 40

+ extend_size=1080

+ expr 7456 - 16 - 8 - 1080 + 40

+ data_size=6392

+ [ 0 -eq 1 ]

+ dd if=/dev/zero of=/dev/mmcblk0 bs=1024 count=1

1+0 records in

1+0 records out

1024 bytes (1.0KB) copied, 0.001788 seconds, 559.3KB/s

+ sfdisk --force -uM /dev/mmcblk0

Checking that no-one is using this disk right now ...

OK

Disk /dev/mmcblk0: 238592 cylinders, 4 heads, 16 sectors/track

sfdisk: ERROR: sector 0 does not have an msdos signature

/dev/mmcblk0: unrecognized partition table type

Old situation:

No partitions found

Warning: given size (6392) exceeds max allowable size (6352)

New situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/mmcblk0p1         0+    15     16-     16383+  83  Linux

/dev/mmcblk0p2        16     23      8       8192   83  Linux

/dev/mmcblk0p3        24   1103   1080    1105920    5  Extended

/dev/mmcblk0p4      1104   7495   6392    6545408   83  Linux

/dev/mmcblk0p5        24+   535    512-    524287+  83  Linux

/dev/mmcblk0p6       536+  1047    512-    524287+  83  Linux

/dev/mmcblk0p7      1048+  1055      8-      8191+  83  Linux

/dev/mmcblk0p8      1056+  1063      8-      8191+  83  Linux

Warning: partition 4 extends past end of disk

Successfully wrote the new partition table

Re-reading the partition table ...

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 13090816 extends beyond EOD, truncated

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)

to zero the first 512 bytes:  dd if=/dev/zero of=/dev/foo7 bs=512 count=1

(See fdisk(8).)

+ sfdisk --force -uM /dev/mmcblk0 -N1

Checking that no-one is using th mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

is disk right now ...

mmcblk0: p4 size 13090816 extends beyond EOD, truncated

OK

Disk /dev/mmcblk0: 238592 cylinders, 4 heads, 16 sectors/track

Old situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/mmcblk0p1         0+    15     16-     16383+  83  Linux

/dev/mmcblk0p2        16     23      8       8192   83  Linux

/dev/mmcblk0p3        24   1103   1080    1105920    5  Extended

/dev/mmcblk0p4      1104   7495   6392    6545408   83  Linux

/dev/mmcblk0p5        24+   535    512-    524287+  83  Linux

/dev/mmcblk0p6       536+  1047    512-    524287+  83  Linux

/dev/mmcblk0p7      1048+  1055      8-      8191+  83  Linux

/dev/mmcblk0p8      1056+  1063      8-      8191+  83  Linux

New situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

   Device Boot Start   End    MiB    #blocks   Id  System

/dev/mmcblk0p1         8     15      8       8192   83  Linux

/dev/mmcblk0p2        16     23      8       8192   83  Linux

/dev/mmcblk0p3        24   1103   1080    1105920    5  Extended

/dev/mmcblk0p4      1104   7495   6392    6545408   83  Linux

/dev/mmcblk0p5        24+   535    512-    524287+  83  Linux

/dev/mmcblk0p6       536+  1047    512-    524287+  83  Linux

/dev/mmcblk0p7      1048+  1055      8-      8191+  83  Linux

/dev/mmcblk0p8      1056+  1063      8-      8191+  83  Linux

Warning: partition 4 extends past end of disk

Successfully wrote the new partition table

Re-reading the partition table ...

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 13090816 extends beyond EOD, truncated

If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)

to zero the first 512 bytes:  dd if=/dev/zero of=/dev/foo7 bs=512 count=1

(See fdisk(8).)

UTP: sending Success to kernel for command $ sh -x mksdcard-android.sh /dev/mmcblk0.

utp_poll: pass returned.

UTP: received command '$ ls -l /dev/mmc* '

UTP: executing "ls -l /dev/mmc* "

brw-r-----    1 root     disk      179,   0 Jan  1 00:00 /dev/mmcblk0

brw-r-----    1 root     disk      179,   8 Jan  1 00:00 /dev/mmcblk0boot0

brw-r-----    1 root     disk      179,  16 Jan  1 00:00 /dev/mmcblk0boot1

brw-r-----    1 root     disk      179,   1 Jan  1 00:00 /dev/mmcblk0p1

brw-r-----    1 root     disk      179,   2 Jan  1 00:00 /dev/mmcblk0p2

brw-r-----    1 root     disk      179,   3 Jan  1 00:00 /dev/mmcblk0p3

brw-r-----    1 root     disk      179,   4 Jan  1 00:00 /dev/mmcblk0p4

brw-r-----    1 root     disk      179,   5 Jan  1 00:00 /dev/mmcblk0p5

brw-r-----    1 root     disk      179,   6 Jan  1 00:00 /dev/mmcblk0p6

brw-r-----    1 root     disk      179,   7 Jan  1 00:00 /dev/mmcblk0p7

brw-r-----    1 root     disk      259,   0 Jan  1 00:00 /dev/mmcblk0p8

UTP: sending Success to kernel for command $ ls -l /dev/mmc* .

utp_poll: pass returned.

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ dd if=$FILE of=/dev/mmcblk0p1'

UTP: executing "dd if=$FILE of=/dev/mmcblk0p1"

9644+0 records in

9644+0 records out

4937728 bytes (4.7MB) copied, 0.542027 seconds, 8.7MB/s

UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk0p1.

utp_poll: pass returned.

UTP: received command 'frf'

UTP: closing the file

UTP: sending Success to kernel for command frf.

utp_poll: pass returned.

UTP: received command '$ mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4'

UTP: executing "mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4"

mke2fs 1.41.4 (27-Jan-2009)

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

407200 inodes, 1626112 blocks

0 blocks (0.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=1665138688

50 block groups

32768 blocks per group, 32768 fragments per group

8144 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632

Writing inode tables: done                           

Creating journal (32768 blocks): done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 31 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

UTP: sending Success to kernel for command $ mkfs.ext4 -b 4096 -m 0 /dev/mmcblk0p4.

utp_poll: pass returned.

UTP: received command 'send'

UTP: sending Success to kernel for command send.

UTP: received command '$ tar xf $FILE '

UTP: executing "tar xf $FILE "

UTP: sending Success to kernel for command $ tar xf $FILE .

utp_poll: pass returned.

UTP: received command '$ sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4'

UTP: executing "sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4"

+ mkdir -p /tmp/data

+ mount /dev/mmcblk0p4 /tmp/data

EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)

+ df -k

+ grep /dev/mmcblk0p4

+ awk {print $2}

+ amount=6402176

+ [ -z 6402176 ]

+ stag=6402176

+ sleep 1

+ umount /dev/mmcblk0p4

+ rm -fr /tmp/data

+ stag=6402144

+ kilo=K

+ echo Get disk block size 6402176K

Get disk block size 6402176K

+ amountkilo=6402144K

+ echo Resize to 6402144K

Resize to 6402144K

+ e2fsck -f /dev/mmcblk0p4

e2fsck 1.41.4 (27-Jan-2009)

Pass 1: Checking inodes, blocks, and sizes

Pass 2: Checking directory structure

Pass 3: Checking directory connectivity

Pass 4: Checking reference counts

Pass 5: Checking group summary information

/dev/mmcblk0p4: 11/407200 files (0.0% non-contiguous), 61906/1626112 blocks

+ resize2fs /dev/mmcblk0p4 6402144K

resize2fs 1.41.4 (27-Jan-2009)

Resizing the filesystem on /dev/mmcblk0p4 to 1600536 (4k) blocks.

The filesystem on /dev/mmcblk0p4 is now 1600536 blocks long.

UTP: sending Success to kernel for command $ sh -x mk-encryptable-data-android.sh /dev/mmcblk0 /dev/mmcblk0p4.

utp_poll: pass returned.

UTP: received command '$ mkfs.ext4 /dev/mmcblk0p5'

UTP: executing "mkfs.ext4 /dev/mmcblk0p5"

mke2fs 1.41.4 (27-Jan-2009)

Filesystem label=

OS type: Linux

Block size=1024 (log=0)

Fragment size=1024 (log=0)

131072 inodes, 524284 blocks

26214 blocks (5.00%) reserved for the super user

First data block=1

Maximum filesystem blocks=67633152

64 block groups

8192 blocks per group, 8192 fragments per group

2048 inodes per group

Superblock backups stored on blocks:

        8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409

Writing inode tables: done                           

Creating journal (8192 blocks): done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 31 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p5.

utp_poll: pass returned.

UTP: received command '$ mkfs.ext4 /dev/mmcblk0p6'

UTP: executing "mkfs.ext4 /dev/mmcblk0p6"

mke2fs 1.41.4 (27-Jan-2009)

Filesystem label=

OS type: Linux

Block size=1024 (log=0)

Fragment size=1024 (log=0)

131072 inodes, 524284 blocks

26214 blocks (5.00%) reserved for the super user

First data block=1

Maximum filesystem blocks=67633152

64 block groups

8192 blocks per group, 8192 fragments per group

2048 inodes per group

Superblock backups stored on blocks:

        8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409

Writing inode tables: done                           

Creating journal (8192 blocks): done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 22 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p6.

utp_poll: pass returned.

UTP: received command 'frf'

UTP: closing the file

UTP: sending Success to kernel for command frf.

utp_poll: pass returned.

UTP: received command '$ mkfs.ext4 /dev/mmcblk0p7'

UTP: executing "mkfs.ext4 /dev/mmcblk0p7"

mke2fs 1.41.4 (27-Jan-2009)

Filesystem label=

OS type: Linux

Block size=1024 (log=0)

Fragment size=1024 (log=0)

2048 inodes, 8188 blocks

409 blocks (5.00%) reserved for the super user

First data block=1

Maximum filesystem blocks=8388608

1 block group

8192 blocks per group, 8192 fragments per group

2048 inodes per group

Writing inode tables: done                           

Creating journal (1024 blocks): done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 20 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk0p7.

utp_poll: pass returned.

UTP: received command 'pipe dd of=/dev/mmcblk0p5 bs=512'

pid is 3676, UTP: executing "dd of=/dev/mmcblk0p5 bs=512"

UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p5 bs=512.

UTP: received command 'frf'

573440+0 records in

573440+0 records out

293601280 bytes (280.0MB) copied, 25.900929 seconds, 10.8MB/s

UTP: closing the file

UTP: sending Success to kernel for command frf.

utp_poll: pass returned.

UTP: received command 'pipe dd of=/dev/mmcblk0p2 bs=512'

pid is 3678, UTP: executing "dd of=/dev/mmcblk0p2 bs=512"

UTP: sending Success to kernel for command pipe dd of=/dev/mmcblk0p2 bs=512.

UTP: received command 'frf'

10720+0 records in

10720+0 records out

5488640 bytes (5.2MB) copied, 0.637624 seconds, 8.2MB/s

UTP: closing the file

UTP: sending Success to kernel for command frf.

utp_poll: pass returned.

UTP: received command '$ echo Update Complete!'

UTP: executing "echo Update Complete!"

Update Complete!

UTP: sending Success to kernel for command $ echo Update Complete!.

utp_poll: pass returned.

消息编辑者为:jianhua xu

Tags (4)
1 Solution
2,584 Views
jasonhsu
Contributor III

Thx Raymond and chipexpert, this issue is fixed now with changing initramfs.cpio.gz.uboot in MFGTool.

initramfs.cpio.gz.uboot is a binary file, i'm not sure what happen exactly, but i guess it should be releated with MBR in the 1st 1KB in eMMC.

(before i send the post, the boot config is already set correctly).

Thx a lot for both of your help. ^ ^

View solution in original post

8 Replies
2,585 Views
jasonhsu
Contributor III

Thx Raymond and chipexpert, this issue is fixed now with changing initramfs.cpio.gz.uboot in MFGTool.

initramfs.cpio.gz.uboot is a binary file, i'm not sure what happen exactly, but i guess it should be releated with MBR in the 1st 1KB in eMMC.

(before i send the post, the boot config is already set correctly).

Thx a lot for both of your help. ^ ^

2,584 Views
linhsun
Contributor III

Dear jianhua Xu and all

    I change mfgtool(try different version) and initramfs.cpio.gz.uboot, but always into download mode, have your any suggest? thanks

0 Kudos
Reply
2,584 Views
Yuri
NXP Employee
NXP Employee

Hello,

  the following Community thread may be useful :

 

https://community.nxp.com/thread/312758 

Regards,

Yuri.

0 Kudos
Reply
2,584 Views
devarajgs
NXP Employee
NXP Employee

Hi,

We are also facing similar issue. can you please share the latest initramfs.cpio.gz.uboot file in MFG tool.

What are the changes that are done to the new initramfs.cpio.gz.uboot?

Thanks and Regards,

-Devaraj

0 Kudos
Reply
2,584 Views
jasonhsu
Contributor III

Hi

Anyway, i'm not sure it is help for you, but you can try ^^

2,584 Views
dreaminghell
Contributor I

Dear Jianhua

         Can you send me the Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER soft, I can not downloard it now. My mail is: dreaminghell@163.com. Thanks!

0 Kudos
Reply
2,584 Views
igorpadykov
NXP Employee
NXP Employee

Hi jianhua,

you should close MFG Tool, disconnect USB, power off board.

For booting from eMMC please set correct boot pins, then power-up board,

then provide log from terminal.

Best regards

chip

0 Kudos
Reply
2,584 Views
raymondwang
Senior Contributor I

It seems mfg progress okay!

Did you ever check your EIM boot option config ? Even you flash eMMC device properly, wrong config may cause boot failed ,then enter download mode once again.

0 Kudos
Reply