i.MX6Q SMP in normal world

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q SMP in normal world

Jump to solution
1,510 Views
vsiles
Senior Contributor I

Hi,

I am trying to port  Linux for i.MX6Q (SabreSD with NXP/Freescale's kernel or SabreLite with Boundary Devices kernel, we have the same issue on both) from running in the secure world to the normal world. To make things simple at first:

- we configured the whole board (CSU/AIPSTZ/NSACR, ...) to allow access from secure and non secure world (especially, the SRC is accessible to Linux in the normal world)

- access to cp15/SCU which are impossible from the Normal World have been fixed by issuing smc to our monitor

In this setup:

- original kernel correctly boots Linux in the Secure World with 4 cores running

- patched kernel without SMP support correctly runs Linux in the Normal World with 1 core running

- patched kernel with SMP support runs Linux in the Normal World with only 1 core, the other 3 failed to start (CPUN: failed to come online)

From my experience with QoirQ boards, I realized that we failed at properly configuring the secondary cores, so I added the following configuration to the secure kernel to initialize secondary cores:

- the part of the GICC/GICD only available to the secondary cores are correctly initialized "per core" (SGI/PPI/SPI to non secure, using IRQ, not FIQ)

- NSACR "per core" is set to 0x43FFFF

- Cortex A9 Diagnostic register is set to the same value as core 0

Then the secondary cores enters a waiting loop (based on wfi) waiting for the relevant SRC_GPR register to be setup by Linux. Finally, Linux wakes up the core by sending a wakeup IPI.

With this modification, the secondary cores are coming online (CPUN: Booted secondary processor), but Linux fails (most of the time silently) to boot. The best situation I can reach is (CPU0: stopping is to relevant, it can be CPU1, CPU2, ...)

imx mcc test is registered.

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)

ALSA device list:

  #0: imx6q-sabrelite-sgtl5000

  #1: imx-hdmi-soc

Freeing unused kernel memory: 272K (80841000 - 80885000)

*** Error in `/bin/sh': free(): invalid next size (normal): 0x003e8078 ***

Kernel panic - not syncing: Attempted to kill init! exitcode=0x00007f00

CPU0: stopping

CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.14.28-gb821ffaf-dirty #15

Backtrace:

[<80011ab4>] (dump_backtrace) from [<80011ccc>] (show_stack+0x18/0x1c)

r6:808a1e04 r5:ffffffff r4:00000000 r3:00000000

[<80011cb4>] (show_stack) from [<80633598>] (dump_stack+0x84/0xc4)

[<80633514>] (dump_stack) from [<800148bc>] (handle_IPI+0x178/0x18c)

r6:80884e24 r5:00000005 r4:00000000 r3:80886000

[<80014744>] (handle_IPI) from [<800085a4>] (gic_handle_irq+0x60/0x64)

r8:80886000 r7:f4a00100 r6:80887f30 r5:8088e948 r4:f4a0010c r3:8000f1ec

[<80008544>] (gic_handle_irq) from [<80012840>] (__irq_svc+0x40/0x70)

Exception stack(0x80887f30 to 0x80887f78)

7f20:                                     00000000 00000000 00000001 8001dfa0

7f40: 8088e570 8063b2bc 80886000 808c96eb 80886000 80886000 00000001 80887f84

7f60: 80887f88 80887f78 8000f1ec 8000f1f0 600c0013 ffffffff

r7:80887f64 r6:ffffffff r5:600c0013 r4:8000f1f0

[<8000f1b0>] (arch_cpu_idle) from [<800695cc>] (cpu_startup_entry+0x10c/0x15c)

[<800694c0>] (cpu_startup_entry) from [<8062f428>] (rest_init+0x8c/0x90)

r7:8088e480 r3:80886000

[<8062f39c>] (rest_init) from [<80841bac>] (start_kernel+0x368/0x374)

r4:8088e608 r3:80886000

[<80841844>] (start_kernel) from [<10008074>] (0x10008074)

One time, I got a login prompt, but every key input made the login reset and I could't log in.

I am waiting for Boundary Devices jtag adapter to try to understand what's happening, but if anyone has suggestions on things I might have missed, I would be grateful

Best,

Vincent

Labels (1)
1 Solution
883 Views
vsiles
Senior Contributor I
0 Kudos
3 Replies
884 Views
vsiles
Senior Contributor I
0 Kudos
883 Views
vsiles
Senior Contributor I

I just received my adapter from BD and as soon as I plugged it in, the board rebooted, and linux successfully booted in SMP with 2 cores (I was only releasing 2 cores from Secure State to debug the issue), but the file system was mounted as read only.

See the attached log, there are a couple of errors (mostly No such file or directory) that I don't understand, maybe someone can make sense of all this.

0 Kudos
883 Views
vsiles
Senior Contributor I

And here is a second log where the same boot failed, but lots of "init: failed to lauch ...." happened

0 Kudos