i.MX6Q Reset Lock Up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Reset Lock Up

1,086 Views
PaulDeMetrotion
Senior Contributor I

I am developing a Yocto kernel for a custom device based on the i.MX6Q. This board works fine when powered cold. If I try to reboot the board form the kernel or reset it from the u-boot prompt, it will almost always lock up at the "Starting kernel ..." message. Occasionally it will reboot successfully. Using an emulator, I have determined that the kernel jumps to the panic function but not always from the same spot in the code. Any one seen this issue before?

Is DDR re-initialized after each reset?

Here is my output:

U-Boot 2014.04 (Jan 14 2016 - 09:35:26)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 38 C, calibration data: 0x5534cc69

Reset cause: POR

Board: SBC35-C398Q

Boot Device: SD

I2C:   ready

DRAM:  2 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

Unable to allocate framebuffer memory

In:    serial

Out:   serial

Err:   serial

mmc0 is current device

Net:   Phy not found

FEC

Normal Boot

Hit any key to stop autoboot:  0

reading zImage

5938056 bytes read in 279 ms (20.3 MiB/s)

reading imx6q-c398.dtb

40261 bytes read in 21 ms (1.8 MiB/s)

Kernel image @ 0x10800000 [ 0x000000 - 0x5a9b88 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800cd44

Starting kernel ...

0 Kudos
6 Replies

676 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

DDR is initialized at each reset, it is shown in Table 60-4. SRC reset functionality

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

When ldo bypass (by default LDO bypass is enabled.) is used then

after reset processor will start with lower power supply voltages, than needed.

After reset processor ldos are enabled, while pmic stays in ldo bypass

configuration. For that reason recommended to reset also pmic using PWRON.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

676 Views
PaulDeMetrotion
Senior Contributor I

We are using an external PMPF0100 regulator. Its reset is tied to the same POR reset for the i.MX6Q processor. How should I handle the LDO Bypass when I have an external PMIC?

0 Kudos

676 Views
igorpadykov
NXP Employee
NXP Employee

could you clarify your description "If I try to reboot the board

form the kernel or reset it from the u-boot prompt" .

Is POR&pmic_PWRON are asserted ? On Sabre board spf-27392

it is done with U507 Wdog signal.

~igor

0 Kudos

676 Views
PaulDeMetrotion
Senior Contributor I

Igor,

Where did you go? Are you out of ideas?

0 Kudos

676 Views
PaulDeMetrotion
Senior Contributor I

OK I have resolved this problem by adding the following ldo_mode_set function. Unfortunately I can no longer save my environment variables to the MMC. If I back this function out of the code, I can save my environment variables but cannot reboot. Obviously I am on the right track, but where is the sweet spot where I can do both???

void ldo_mode_set(int ldo_bypass)

{

    unsigned char value;

    int is_400M;

    unsigned char vddarm;

    // increase VDDARM/VDDSOC to support 1.2G chip

    if (check_1_2G()) {

        ldo_bypass = 0; // ldo_enable on 1.2G chip

        printf("1.2G chip, increase VDDARM_IN/VDDSOC_IN\n");

        // increase VDDARM to 1.425V

        if (i2c_read(0x8, 0x20, 1, &value, 1)) {

            printf("Read SW1AB error!\n");

            return;

        }

        value &= ~0x3f;

        value |= 0x2d;

        if (i2c_write(0x8, 0x20, 1, &value, 1)) {

            printf("Set SW1AB error!\n");

            return;

        }

        // increase VDDSOC to 1.425V

        if (i2c_read(0x8, 0x2e, 1, &value, 1)) {

            printf("Read SW1C error!\n");

            return;

        }

        value &= ~0x3f;

        value |= 0x2d;

        if (i2c_write(0x8, 0x2e, 1, &value, 1)) {

            printf("Set SW1C error!\n");

            return;

        }

    }

    // switch to ldo_bypass mode, boot on 800Mhz

    if (ldo_bypass) {

        prep_anatop_bypass();

        // decrease VDDARM for 400Mhz DQ:1.1V, DL:1.275V

        if (i2c_read(0x8, 0x20, 1, &value, 1)) {

            printf("Read SW1AB error!\n");

            return;

        }

        value &= ~0x3f;

        #if defined(CONFIG_MX6DL)

        value |= 0x27;

        #else

        value |= 0x20;

        #endif

        if (i2c_write(0x8, 0x20, 1, &value, 1)) {

            printf("Set SW1AB error!\n");

            return;

        }

        // increase VDDSOC to 1.3V

        if (i2c_read(0x8, 0x2e, 1, &value, 1)) {

            printf("Read SW1C error!\n");

            return;

        }

        value &= ~0x3f;

        value |= 0x28;

        if (i2c_write(0x8, 0x2e, 1, &value, 1)) {

            printf("Set SW1C error!\n");

            return;

        }

        // MX6Q:

        // VDDARM:1.15V@800M; VDDSOC:1.175V@800M

        // VDDARM:0.975V@400M; VDDSOC:1.175V@400M

        // MX6DL:

        // VDDARM:1.175V@800M; VDDSOC:1.175V@800M

        // VDDARM:1.075V@400M; VDDSOC:1.175V@400M

        is_400M = set_anatop_bypass(2);

       

        if (is_400M)

        #if defined(CONFIG_MX6DL)

            vddarm = 0x1f;

        #else

            vddarm = 0x1b;

        #endif

        else

        #if defined(CONFIG_MX6DL)

            vddarm = 0x23;

        #else

            vddarm = 0x22;

        #endif

       

        if (i2c_read(0x8, 0x20, 1, &value, 1)) {

            printf("Read SW1AB error!\n");

            return;

        }

        value &= ~0x3f;

        value |= vddarm;

        if (i2c_write(0x8, 0x20, 1, &value, 1)) {

            printf("Set SW1AB error!\n");

            return;

        }

        // decrease VDDSOC to 1.175V

        if (i2c_read(0x8, 0x2e, 1, &value, 1)) {

            printf("Read SW1C error!\n");

            return;

        }

        value &= ~0x3f;

        value |= 0x23;

        if (i2c_write(0x8, 0x2e, 1, &value, 1)) {

            printf("Set SW1C error!\n");

            return;

        }

        finish_anatop_bypass();

        printf("switch to ldo_bypass mode!\n");

    }

}

0 Kudos

676 Views
PaulDeMetrotion
Senior Contributor I

When I start the board with a power cycle, it will boot successfully 100% of the time. When I reset the board in the following manners, it will boot successfully about 5% of the time. All other attempts stop at the "Starting kernel ..." message.

  1. Reset command from u-boot prompt
  2. Reboot command from kernel prompt
  3. Reset from CPU emulator

I would like to point out that we have a Linux build for this same device using the LTIB tool that works correctly. We are in the process of transitioning to Yocto. It is the Yocto version that does not work.

Is there possibly an issue with our device tree? I have modeled it like the Sabre Auto device. I have the following in our device tree:

&gpc {

    fsl,ldo-bypass = <0>;

    fsl,wdog-reset = <1>;

};

0 Kudos