i.MX6Q PCI Express Endpoint Bass Address Boundary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6Q PCI Express Endpoint Bass Address Boundary

458件の閲覧回数
masamiyasui
Contributor I

We would like to use i.MX 6Q as the PCI Express endpoint.
Please tell us about the boundary of the address of the local memory assigned to BAR.

48.12.45 iATU Region Lower Base Address Register
(PCIE_PL_iATURLBA)
 
Is not this register setting 64 KB boundary?

It seems that it will not work unless we set the same boundary as the BAR capacity (BAR_MASK).

Is this specification of iATU?

Note: We are using iATU in BAR Mode.

48.12.44 iATU Region Control 2 Register (PCIE_PL_iATURC 2)
Bit 30 Match_Mode = 1 (BAR Mode)

ラベル(2)
0 件の賞賛
返信
1 返信

395件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   According to Table 48-20 (Configuration Parameters Relevant to Address Translation)

of i.MX6 D/Q RM (Rev. 4, 09/2017):

CX_ATU_MIN_REGION_SIZE (Minimum Size of Address Translation Region) is 64 kB.

  Note, from i.MX6 D/Q RM (section 48.10.5 [BAR 0 Mask Register (PCIE_EP_MASK0)]):

The core requires each memory BAR to claim at least 4 KB. The core requires each I/O

BAR to claim at least 256 bytes.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信