i.MX6Q PCI Express Endpoint Bass Address Boundary

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q PCI Express Endpoint Bass Address Boundary

426 Views
masamiyasui
Contributor I

We would like to use i.MX 6Q as the PCI Express endpoint.
Please tell us about the boundary of the address of the local memory assigned to BAR.

48.12.45 iATU Region Lower Base Address Register
(PCIE_PL_iATURLBA)
 
Is not this register setting 64 KB boundary?

It seems that it will not work unless we set the same boundary as the BAR capacity (BAR_MASK).

Is this specification of iATU?

Note: We are using iATU in BAR Mode.

48.12.44 iATU Region Control 2 Register (PCIE_PL_iATURC 2)
Bit 30 Match_Mode = 1 (BAR Mode)

Labels (2)
0 Kudos
Reply
1 Reply

363 Views
Yuri
NXP Employee
NXP Employee

Hello,

   According to Table 48-20 (Configuration Parameters Relevant to Address Translation)

of i.MX6 D/Q RM (Rev. 4, 09/2017):

CX_ATU_MIN_REGION_SIZE (Minimum Size of Address Translation Region) is 64 kB.

  Note, from i.MX6 D/Q RM (section 48.10.5 [BAR 0 Mask Register (PCIE_EP_MASK0)]):

The core requires each memory BAR to claim at least 4 KB. The core requires each I/O

BAR to claim at least 256 bytes.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply