Hi all
We'd like to design a customized board which support 4GB DDR3 RAM.
We use it in Linux BSP 4.1.0, but it seems only 1GB and 2GB DDR3 codes we can refer .
Before I use 4G bits (1CS) *4,total memory is 2G bytes is ok for me.
The DDR3 is H5TQ4G63AFR.
Now my board total memory is 4G bytes, 4G bits (2CS) *8. Per CS is 4ps.
Unfortunately, we got error when we try to use DDR stress tester on 4GB ram board.
error is here:
Beginning stress test
loop: 1
DDR Freq: 528 MHz
t0.1: data is addr test
Address of failure: 0x90000000
Data was: 0x00000200
But pattern should match address
We will attached my detail log and my test tools.
How to design hardware about have eight ddr3 chips,4Gbits(per chip is 256MB*16)*8?
Any ideas can help me to solve this issues?
Thanks a lot.
Leo
Original Attachment has been moved to: imx6q_4g.inc.zip
Original Attachment has been moved to: ddr3_test_log.txt.zip
Original Attachment has been moved to: DDR_Stress_Tester_V1.0.3.zip
Hi Leo
first please recheck what is processor: Q or DL,
since DL supports frequencies up to 400MHz only.
Also just for reference one can look at attached 4GB i.MX6Q
init script example with 8xMT41J128M16HA.
Error means that processor wrote 0x90000000 data to
address 0x90000000 but read back data = 0x00000200
that means some basic errors: for example layout error or broken lines.
One can check that with oscilloscope and SDK i.MX 6Series Platform SDK
(it has simple DDR test), probably one can use attached init script with low frequency
(it is not optimized for H5TQ4G63AFR but should work well on low frequencies too).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
First my processor is imx6q that it supports frequencies up to 528Mhz.
I think the layout maybe have not problem.
if use 1 cs0 then I test the same board,ddr test tool can test passed ok in 528Mhz to 629Mhz.
if use 2cs(cs0 and cs1) can not pass ok and 400Mhz also not ok.
May be the connection graph design of DDR3 is not ok?
Can I have a look your connection graph design of DDR3?