i.MX6Q DDR3 clock problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q DDR3 clock problem

Jump to solution
805 Views
cbrust
Contributor III

For troubleshooting purposes, we generated a script to initialize DDR3 to use a 400MHz (instead of 533MHz) clock using the v1.9 Freescale Register Aid tool (latest as of 12/5/15).  We verified the 400MHz initialization script was indeed different from a 533MHz script generated by the same tool.  However, after using the 400MHz script to initialize DDR, the clock frequency remains at 533MHz by o-scope measurement (we saw this issue before with the old register scripting aid too).  Because the clock frequency does not change there is no way we can try a lower frequency for troubleshooting our DDR3.  Is there something additional that needs to be done in order to get the 400MHz clock frequency or is this an indication of a larger issue with our i.MX6Q?

Labels (2)
0 Kudos
Reply
1 Solution
686 Views
igorpadykov
NXP Employee
NXP Employee

Hi C

generated script just calculates MMC/DDR settings but does not set CCM frequencies.

This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.

So there are no indication of any  issues with your i.MX6Q.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
686 Views
Yuri
NXP Employee
NXP Employee

You may create SR to get some example sources how to change frequency.

Regards,

Yuri.

0 Kudos
Reply
687 Views
igorpadykov
NXP Employee
NXP Employee

Hi C

generated script just calculates MMC/DDR settings but does not set CCM frequencies.

This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.

So there are no indication of any  issues with your i.MX6Q.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
686 Views
cbrust
Contributor III

Thanks Igor.

We figured we were missing something simple or making a bad assumption.

Cliff

0 Kudos
Reply