i.MX6Q DDR3 clock problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX6Q DDR3 clock problem

跳至解决方案
802 次查看
cbrust
Contributor III

For troubleshooting purposes, we generated a script to initialize DDR3 to use a 400MHz (instead of 533MHz) clock using the v1.9 Freescale Register Aid tool (latest as of 12/5/15).  We verified the 400MHz initialization script was indeed different from a 533MHz script generated by the same tool.  However, after using the 400MHz script to initialize DDR, the clock frequency remains at 533MHz by o-scope measurement (we saw this issue before with the old register scripting aid too).  Because the clock frequency does not change there is no way we can try a lower frequency for troubleshooting our DDR3.  Is there something additional that needs to be done in order to get the 400MHz clock frequency or is this an indication of a larger issue with our i.MX6Q?

标签 (2)
0 项奖励
回复
1 解答
683 次查看
igorpadykov
NXP Employee
NXP Employee

Hi C

generated script just calculates MMC/DDR settings but does not set CCM frequencies.

This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.

So there are no indication of any  issues with your i.MX6Q.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
683 次查看
Yuri
NXP Employee
NXP Employee

You may create SR to get some example sources how to change frequency.

Regards,

Yuri.

0 项奖励
回复
684 次查看
igorpadykov
NXP Employee
NXP Employee

Hi C

generated script just calculates MMC/DDR settings but does not set CCM frequencies.

This should be done using jtag, in DDR Tester (input DDR requency) or using other ways.

So there are no indication of any  issues with your i.MX6Q.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
683 次查看
cbrust
Contributor III

Thanks Igor.

We figured we were missing something simple or making a bad assumption.

Cliff

0 项奖励
回复