Hello Champs,
From HDG, "Table 2-7. Oscillator and clock recommendations" wrote;
2. External kilohertz source
"The RTC_XTALI signal should not be driven if the VDD_SNVS_CAP supply is off"
Could you explain the purpose of this restriction?
My customer is thinking to use VDD_SNVS_IN from PF0100, dropping to 1.0V to provide power with the external 32KHz clock circuit.
Since VDD_SNVS_CAP is generated from VDD_SNVS_IN with some delay, might there be a condition which applies the above restriction?
Best regards,
Nori Shinozaki
已解决! 转到解答。
Hi Nori
your precautions are justified, yes one needs first to
apply VDD_SNVS_CAP, then provide clock. If necessary one can
add delay to external 32KHz clock circuit.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nori
your precautions are justified, yes one needs first to
apply VDD_SNVS_CAP, then provide clock. If necessary one can
add delay to external 32KHz clock circuit.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------