i.MX6DQ: When to provide power with external 32KHz clock cirtuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ: When to provide power with external 32KHz clock cirtuit

Jump to solution
560 Views
norishinozaki
Contributor V

Hello Champs,

From HDG, "Table 2-7. Oscillator and clock recommendations" wrote;

2. External kilohertz source

"The RTC_XTALI signal should not be driven if the VDD_SNVS_CAP supply is off"

Could you explain the purpose of this restriction?

My customer is thinking to use VDD_SNVS_IN from PF0100, dropping to 1.0V to provide power with the external 32KHz clock circuit.

Since VDD_SNVS_CAP is generated from VDD_SNVS_IN with some delay, might there be a condition which applies the above restriction?

Best regards,

Nori Shinozaki

Labels (2)
0 Kudos
1 Solution
496 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

your precautions are justified, yes one needs first to

apply VDD_SNVS_CAP, then provide clock. If necessary one can

add delay to external 32KHz clock circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
497 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nori

your precautions are justified, yes one needs first to

apply VDD_SNVS_CAP, then provide clock. If necessary one can

add delay to external 32KHz clock circuit.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
496 Views
norishinozaki
Contributor V

Hello Igor,

Thanks always!

Best regards,

Nori Shinozaki

0 Kudos