i.MX6DQ IPU IC combining performance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ IPU IC combining performance.

ソリューションへジャンプ
612件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL IPU CSI.

Please see the slide No. 56 of attached file in A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

It says the combining in the Image Conveter is upt to 40M pixels/sec with i.MX6DQ.

Next, please see chapter 37.1.2.1.5.3 in IMX6DQRM Rev.3, it says the IC perfomance is 200M pixels/sec for input and 100M pixels/sec for output.

To understand combining performance by Image Converter, which performance should I use?

Best Regards,

Satoshi Shimoda

ラベル(5)
タグ(4)
0 件の賞賛
1 解決策
484件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
485件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛