I cannot find detailed description of RX_EQ[2:0] bits in RX_OVRD_IN_HI register in neither chip errata nor reference manual. I think RX_OVRD_IN_HI[RX_EQ_OVRD] enables overriding PCIe2 Rx equalizer setting by RX_EQ[2:0] bit. But what does each RX_EQ[2:0] value mean?
Hello Yutaka Ando,
My apologies for the delay. The RX_EQ refers to the PCIe equalizer settings which result in an adaptive filter. The RX_EQ would be one of the coefficients for this filter.
The possible RX_EQ values should be generated trough equalization training to obtain the optimal value, similarly to calibration on the DDR3 standard.
I hope that this helps!
Regards,
Hello gusarambula,
Thank you for the answer.
The possible RX_EQ values should be generated trough equalization training to obtain the optimal value,
What register holds the equalization training? PCIE_PHY_RX_ASIC_IN?
If so, the actual procedure of the workaround for ERR004489 will be
1. read a value from PCIE_PHY_RX_ASIC_IN[RX_EQ]
2. write the value to RX_OVRD_IN_HI[RX_EQ] with RX_OVRD_IN_HI[RX_EQ_OVRD]
Is this correct?