i.MX6DC MMDC 1T/2T.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DC MMDC 1T/2T.

1,423件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about i.MX6DQ MMDC.

They want to know how many clock cycle the MMDC speds to send a command to a DRAM (1T or 2T).

http://www.overclockers.com/forums/showthread.php/690464-What-is-1T-2T

Would you let me know it?

And if change the number of cycles, would you let me know how change it also?

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
0 件の賞賛
返信
11 返答(返信)

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

seems for i.MX6DQ MMDC similar parameter would be RALAT,

defined as 5 in ddr initialization scripts for nxp reference boards.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,222件の閲覧回数
satoshishimoda
Senior Contributor I

Dear Igor,

RALAT seems to be used for read access, not issue a command.

So I feet it is different from the 1T/2T.

I think tMRD in MMDCx_MDCFG1 register is the one.

Do you think so?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

to answer on that it is neceesary to know

accurate "1T/2T" definition. What document describes it ?

Also seems this parameter is from another processor

architecture, what is the reason to consider or use it

in regard to i.MX?

Best regards

igor

0 件の賞賛
返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I believe these settings are not applicable directly

to i.MX6 MMDC and there is no similar parameter for them.

Mentioned documents related to PowerQUICC memory controllers

which support memory DIMM and has such parameter in its memory controller

registers. I.MX6 memory controller MMDC has not special settings

for DIMM memories.

Regarding signal integrity simulation please use ibis model.

IBIS Model (1)

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP

Best regards

igor

0 件の賞賛
返信

1,222件の閲覧回数
satoshishimoda
Senior Contributor I

Dear Igor,

OK, I understand there is no same parameter for i.MX6DQ.

So would you let me know the command length (1 cycle or 2 cycles) at least?

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I am not aware of cases where such kind of memory

was used with i.MX6 MMDC. As this memory is not standard

memory which could be supported by i.MX6, suggest

to escalate it with local fae or use professional services.

Note, additional support may be provided based on project

opportunity.

Best regards

igor

0 件の賞賛
返信

1,222件の閲覧回数
satoshishimoda
Senior Contributor I

Dear Igor,

Sorry for my unsufficient explanation, my last question mentioned about general DDR3, not DIMM.

I understand the command length is 1 cycle to satisfy JEDEC, right?

Best Regards

Satoshi Shimoda

0 件の賞賛
返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

could you say where in JEDEC

document is described parameter which you are

interested in. I looked at  JESD79 DDR3 specs but could

not find 1T/2T parameter.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,222件の閲覧回数
satoshishimoda
Senior Contributor I

Dear Igor,

Yes, JEDEC specification does not mentioned 1T/2T parameter as you said.

But the command length seems to be 1 cycle according to Figure 5, 6, 7, etc...

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信

1,222件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

"1T/2T parameter" is used by dim memories

DIMM - Wikipedia, the free encyclopedia

these modules usually are not used in i.MX6 designs,

there are no special "1T/2T' settings for them.

If you wsh to know how support them, suggest to escalate

with local fae for special support.

Best regards

igor

0 件の賞賛
返信