i.MX6 dual appearance in JTAG chain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 dual appearance in JTAG chain

1,296件の閲覧回数
joachimhofmann
Contributor I

Dear NXP Team,

we like to understand how a i.MX6 dual  normally and correctly appears in the JTAG chain,

I have a customer with the attached list of devices while only two ICs are actually JTAG connected, one Xilinx CPLD and the i.MX6D processor.

3 instances are presumably associated with the i.MX

1. Freescale/Motorola

2. unidentified ??

3. ARM

Please clarify how the i.MX6D SHOULD appear (how many and which instances) and also advise if the use of a foreign third party JTAG tool could be the cause.
In this case: Which JTAG tools are recommended or approved

With regards

Joachim Hofmann

タグ(1)
0 件の賞賛
3 返答(返信)

1,095件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joachim

please check sect.7.4 Defining the JTAG chain  attached i.MX6 Hardware Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,095件の閲覧回数
joachimhofmann
Contributor I

Hi Igor,

thanks, but your Reply did not contain an attachment or a link to a document.

The "Hardware user Guide" for i.MX6D makes no mention of "JTAG chain" in section 7.4 (which talks about IBIS model).

Please include a link or the actual document you are refferring to.

With regards

Joachim

0 件の賞賛

1,095件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Joachim

attachment in red in previous answer (IMX6DQ6SDLHDG.pdf), please click with mouse on it

pastedImage_1.jpg

Best regards
igor

0 件の賞賛