i.MX6 and jitter for audio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6 and jitter for audio

1,002 次查看
philippev
Contributor I

Hi all, we use i.MX6 for audio application. i.MX6 generate master clock for bit rate like 44.1 for audio cd quality.

We use PLL4 (also referred to as an Audio PLL) - This is a fractional multiplier PLL used

for generating a low jitter and high precision audio clock with standardized audio

frequencies. The PLLs oscillator frequency range is from 650MHz to 1300MHz, and

the frequency resolution is better than 1Hz. This clock is mainly used as a clock for

serial audio interfaces and as a reference clock for external audio codecs. It is

equipped with a divider on its output and can generate divided by 1, 2 or 4 from the

PLL VCO frequency.

Question we have a low jitter, but we want to quantify this value (nano sec , pico sec) ?

Tks.


标签 (3)
0 项奖励
回复
2 回复数

753 次查看
sinanakman
Senior Contributor III

Hi Philippe, does this document help : cache.freescale.com/files/32bit/doc/app_note/AN4952.pdf 

Regards

Sinan Akman

0 项奖励
回复

753 次查看
philippev
Contributor I

tanks

0 项奖励
回复