i.MX6 a AUDMUX port can supply a signal to other two ports at the same time?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 a AUDMUX port can supply a signal to other two ports at the same time?

ソリューションへジャンプ
576件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 AUDMUX.

I want to know whether a AUDMUX port can supply a signal (e.g. TFS, TCK) to other two ports at the same time (= without internal network mode) as the following image?

pastedImage_3.png

Is it possible?

Best Regards,

Satoshi Shimoda

ラベル(7)
タグ(1)
0 件の賞賛
返信
1 解決策
422件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes such configuration is possible

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
423件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes such configuration is possible

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信