i.MX6 a AUDMUX port can supply a signal to other two ports at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 a AUDMUX port can supply a signal to other two ports at the same time?

Jump to solution
575 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 AUDMUX.

I want to know whether a AUDMUX port can supply a signal (e.g. TFS, TCK) to other two ports at the same time (= without internal network mode) as the following image?

pastedImage_3.png

Is it possible?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
421 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes such configuration is possible

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
422 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes such configuration is possible

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply