i.MX6-ULL multiple DDR3 chips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6-ULL multiple DDR3 chips

426 Views
JMerrill79
Contributor I

We are looking at designing around the ULL and utilizing the Win 10 IOT BSP.  Design constraints have a lot to do with power consumption.  We got the win 10  BSP running on the EVK but based on performance of the RAM viewing it through the Windows Device Portal it appears that the majority of the RAM is consumed.  If we use the ULL we will need to expand the RAM to the maximum capability.

Per the ULL hardware development guide  section 3.5:

"The chip can support up to 2 GB of DRAM memory. i.MX 6ULL DDR routing needs to be separated into
three groups: data, address, and control. Each group has its own method of routing from an i.MX 6 series chip to DDR memory. The DDR layout has 2 Gbyte and 1 Gbyte options."

How are these 2 options accomplished accomplished?  I can find no examples in the developers guide, Community forum, or other online resources.  Can I use 4 chips at 8Gb (512M x 16) or would we be limited to 2 chips at 16Gb (1G x 16)? 

Should we look to another design guide for explanation (like the SoloX HW design guide)? Can we look at the other EVK's in the I/MX6 family for reference (SoloX, Quad)?

 

 

Labels (1)
0 Kudos
1 Reply

417 Views
igorpadykov
NXP Employee
NXP Employee

Hi JMerrill79

 

>Can I use 4 chips at 8Gb (512M x 16) or would we be limited to 2 chips at 16Gb (1G x 16)? 

 

i.MX6ULL MMDC has two chip selects, x16 data bus width, supported densities

256 Mbits–8 Gbits as described in Table 35-1. MMDC feature summary

i.MX 6ULL Applications Processor Reference Manual

So seems "4 chips at 8Gb (512M x 16)" can not be used.

 

>Should we look to another design guide for explanation (like the SoloX HW design guide)?

>Can we look at the other EVK's in the I/MX6 family for reference (SoloX, Quad)?

 

yes as MMDC module is the same.

 

Best regards
igor

0 Kudos