i.MX6-UL/PF300x Orcad/Altium Symbol

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6-UL/PF300x Orcad/Altium Symbol

1,636 次查看
ulrichschmidt
Contributor I

Dear Freescale Support Community,

to start with a i.MX6-UL design, can you provide me with the symbol data to edit the schematics for the

- i.MX6-UL (14x14) and

- PF300x

Design tool is Altium, so if you can export from Orcad 16.2 is highly appreciated.

Best regards,

Uli

标签 (1)
0 项奖励
回复
2 回复数

946 次查看
art
NXP Employee
NXP Employee

Please find attached the schematic of the iMX6UL EVK CPU module in OrCAD 16.2 format where the symbol can be extracted from. Unfortunately, no OrCAD schematic of the PF3000 EVM board is available in public access.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

946 次查看
marco_cassol
NXP Employee
NXP Employee

Hi Uli,

Create a Service Request under Sales and Support|Freescale  to request the information you need.

Please copy me as CC to it.

Regards,

Marco

0 项奖励
回复