i.MX6 SD Card maximum PCB Track Lenghts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 SD Card maximum PCB Track Lenghts

Jump to solution
5,746 Views
skuzu
Contributor II

Hello,

Question about the maximum PCB signal track lengths for the SD interface :

Because of the tight PCB space and other mechanical limitations, the best we can place the Micro SD connector is 3.5 inches away from the i.MX6 DualLite. Which makes the SD track lengths around 4 inches long. We would like to run the SD interface at SDR12 speed (25MHz).

Is 4 inches of track length acceptable for SD interface to work at 25MHz?

regards,

Selcuk

Labels (2)
0 Kudos
1 Solution
1,690 Views
igorpadykov
NXP Employee
NXP Employee

Hi Selcuk

length is acceptable. SD Layout guidelines can be found on

sect.6 SD/MMC/SDIO Card and SPI interfaces, 5.3 Minimizing Reflections

AN4215 http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf

Best regards

igor
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
1,691 Views
igorpadykov
NXP Employee
NXP Employee

Hi Selcuk

length is acceptable. SD Layout guidelines can be found on

sect.6 SD/MMC/SDIO Card and SPI interfaces, 5.3 Minimizing Reflections

AN4215 http://cache.freescale.com/files/32bit/doc/app_note/AN4215.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos