i.MX6 Power requirement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 Power requirement

688件の閲覧回数
saurabh206
Senior Contributor III

Hi

I want to know about power of i.MX6 processor.

I want to select chip based on low power requirement.

Thanks

Saurabh

ラベル(1)
タグ(2)
0 件の賞賛
3 返答(返信)

561件の閲覧回数
pankajrana
Contributor III

Hi Saurabh,

For this, one must finalize the interfaces/features required in the end application.

i.Mx6 Sololite would be a good fit for low power requirements.

Also, you may go for UltraLite device as well but it totally depends on the end application/features you require.

Regards,

Pankaj Rana

0 件の賞賛

561件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

561件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

please check sect.4.1.5 Maximum Supply Currents

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

For other i.MX6 one can find similar data in its datasheets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------