i.MX6 Power requirement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Power requirement

679 Views
saurabh206
Senior Contributor III

Hi

I want to know about power of i.MX6 processor.

I want to select chip based on low power requirement.

Thanks

Saurabh

Labels (1)
Tags (2)
0 Kudos
3 Replies

552 Views
pankajrana
Contributor III

Hi Saurabh,

For this, one must finalize the interfaces/features required in the end application.

i.Mx6 Sololite would be a good fit for low power requirements.

Also, you may go for UltraLite device as well but it totally depends on the end application/features you require.

Regards,

Pankaj Rana

0 Kudos

552 Views
BiyongSUN
NXP Employee
NXP Employee

552 Views
igorpadykov
NXP Employee
NXP Employee

Hi Saurabh

please check sect.4.1.5 Maximum Supply Currents

i.MX6DQ Datasheet (rev.4, 7/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

For other i.MX6 one can find similar data in its datasheets.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------