I check the table 8 in IMX6SDLCEC.pdf and find there are the different supply operating ranges in different run modes(LDO Enable and LDO Bypassed). I can not find any description about the two modes in other documents but IMX6SDLRM.pdf, but there are 4 different modes : Internal Bypass,External Bypass,Power Gate,Analog regulation mode.
1, How to understand the difference?
2, Which one is the default mode for the core? LDO Enable or LDO Bypassed mode?
3, If the default mode is LDO Bypassed mode, and we need set the LDO Enable mode, how to design the VDD_ARM_IN and VDD_SOC_IN circuit?
I have checked the reference design in [SPF-27516_C3.pdf]. And, I find VDD_ARM_IN = VDD_SOC_IN = 1.375V, which is not fit the LDO Bypassed mode operating range.
4, How to change the run modes?
I find the information as below:
TRAG==0x1F internal bypass mode
TRAG==0x00 POWER GATE mode
but I don't know what is the TRAG. How to find it?
解決済! 解決策の投稿を見る。
hi,
I have same problem,could you tell me How to change the run modes .when I boot the system, the uboot print "switch ldo bypass mode ",so what should I do to change the mode to ldo_enable mode.
thanks
Hi 王 剑翰
LDO Enable or LDO Bypassed mode are changed
with field REGx_TARG (Bypassed mode =
11111 Power FET switched full on. No regulation.
POWER GATE mode =00000 Power gated off, others =LDO Enable - this is default)
sect.50.7.4 Digital Regulator Core Register (PMU_REG_CORE) IMX6DQRM
How this is implemented in software:
https://gitorious.org/u-mobo/uboot-imx/commit/9b8b6f2ac34c795fbb272b31a2d37aea30ba06f6
For yocto use dts files: ldo-bypass dts, ldo-enable dts
Commits · embest-tech/meta-fsl-arm · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your kindly answer.
Someone tell me the Linux BSP will set as LDO Bypassed mode first, and then change to LDO Enable mode.
If we want to always use LDO Enable mode, we need add like "ldo_active=on" in u-boot . Is it right?
Besides, as you said above, the LDO Bypassed mode IS the Internal Bypass mode and the LDO Enable mode IS the other two modes except POWER GATE mode. I don't know why the same mode has different name in different document?
Hi 王 剑翰
no, linux does not change LDO Bypassed mode first
and then change to LDO Enable mode, in fact this configuration is passed
from uboot to kernel. Linux does not change it.
Regarding different naming, yes this can be noticed in documentation.
You should carefully read documents and fully understand what it is
implied.
Best regards
igor
Hi Igor,
Thank you for your help.
Then, if I add "ldo_active=on" in kernel command line, the LDO enable mode will be set and if I change it as "ldo_active=off", it will enter the LDO Bypassed mode. Right?
Then, if I don't add "ldo_active=on" or "ldo_active=off" in kernel command line, which mode is the default? Is it the LDO Bypassed mode?
Thank you & Best regards!
Hi 王 剑翰
yes, right. Default is LDO enable mode
Best regards
igor
Hi,
Sorry, I check the attached file p.9 and find: it claims the default mode is bypassed mode, not the enable mode you said. But I also think your said is not wrong as I checked the REGx_TARG field and it do show the enable mode is default. I am confused about it. Maybe, I also don't quite understand it. Could you help me again for it ?
Thank you!
You are corect: REGx_TARG field - it do show the enable mode is default
For software BSP it does not make sense - since it depends on used BSP.
Hi,
Sorry to trouble you again.
As the attached file p.9 said:
By defaut, LDO bypass is enabled. If you want to use internal LDO, please specify " ldo_active=on" to the kernel command line. LDO bypass can only be enabled on the board that mounted with external PMIC to supply VDDARM_IN/VDDSOC_IN power rail. LDO bypass is not supported on the chips with 1.2Ghz max CPU frequency.
As above said, if there is no PMIC on the board, the LDO bypass feature cannot be supported. So, in this case, the default mode is LDO enable mode? Right?
But why do you say "if don't use PMIC in design, one needs add "ldo_active=on" in kernel command line."
Hi
from hardware point of view: check REGx_TARG field and it does show the LDO enable mode is default.
Form software point of view this question does not make sense. For example
if you are using Linux L3.0.35_4.1.0_ER_SOURCE - yes here by default, LDO bypass is enabled.
For other BSPs this may be wrong.
So it may be recommended to read carefully BSP dcumentation and find which one is correct.
~igor
Sorry, igor.
You may mistake my question. My question is for the bold type words.
As it says, if there is no PMIC on the board, the LDO bypass feature cannot be supported. I don't know why? As you said, the modes depends on used BSP. So, I think, if the BSP support LDO bypassed mode, the board will support the LDO bypass feature although there is no PMIC on the board.
Yes, If there is no PMIC on the board, the LDO bypass feature cannot be supported
because somebody should regulate voltages for processor, since Freescale linux BSP
CPUFREQ device driver changes voltages.
Form software point of view this question does not make sense, since
for some other custom BSPs this may be wrong.
Hi,
Sorry to trouble you again.
I want to ask you another question:
If we don't use PMIC in our design, whether we need add "ldo_active=on" in kernel command line?
As we don't use PMIC and we set VDD_ARM_IN = VDD_SOC_IN = 1.425V, we don't want it enter LDO Bypassed mode.
Thank you & Best regards!
yes, if don't use PMIC in design, one needs add "ldo_active=on" in kernel command line.
~igor
Could you kindly expain this to me ? Why? I don't quite understand it.
As you said, the LDO enable mode is the default mode. Why I need add "ldo_active=on" in kernel command line to set the LDO enable mode?
Thank you!
I believe actually this depends on specific BSP, for example refer to
attached file p.9 and link below
https://gitorious.org/u-mobo/uboot-imx/commit/9b8b6f2ac34c795fbb272b31a2d37aea30ba06f6
~igor
Hi Igor,
Thank you for your help!
Best regards.