1. After I insert wifi mini-pcie card, the console displays error message:
imx6q-pcie 1ffc000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
pci_bus 0000:00: root bus resource [bus 00-ff]
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
pci 0000:00:00.0: BAR 8: assigned [mem 0x01100000-0x011fffff]
pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]
pci 0000:00:00.0: BAR 7: assigned [io 0x1000-0x1fff]
pci 0000:01:00.0: BAR 2: assigned [mem 0x01100000-0x01103fff 64bit]
pci 0000:01:00.0: BAR 0: assigned [io 0x1000-0x10ff]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
pci 0000:00:00.0: bridge window [mem 0x01100000-0x011fffff]
------------[ cut here ]------------
WARNING: CPU: 0 PID: 1 at kernel/irq/manage.c:1412 request_threaded_irq+0xfc/0x124()
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.14.28-svn1420 #1
[<80015638>] (unwind_backtrace) from [<80011714>] (show_stack+0x10/0x14)
[<80011714>] (show_stack) from [<806801a8>] (dump_stack+0x7c/0xbc)
[<806801a8>] (dump_stack) from [<8002d9a8>] (warn_slowpath_common+0x70/0x8c)
[<8002d9a8>] (warn_slowpath_common) from [<8002da60>] (warn_slowpath_null+0x1c/0x24)
[<8002da60>] (warn_slowpath_null) from [<80069f94>] (request_threaded_irq+0xfc/0x124)
[<80069f94>] (request_threaded_irq) from [<802cba38>] (pcie_pme_probe+0x98/0x1b4)
[<802cba38>] (pcie_pme_probe) from [<802c9448>] (pcie_port_probe_service+0x38/0x84)
[<802c9448>] (pcie_port_probe_service) from [<8034c778>] (driver_probe_device+0x110/0x24c)
[<8034c778>] (driver_probe_device) from [<8034ad7c>] (bus_for_each_drv+0x64/0x98)
[<8034ad7c>] (bus_for_each_drv) from [<8034c638>] (device_attach+0x74/0x88)
[<8034c638>] (device_attach) from [<8034bcbc>] (bus_probe_device+0x84/0xa8)
[<8034bcbc>] (bus_probe_device) from [<8034a138>] (device_add+0x450/0x538)
[<8034a138>] (device_add) from [<802c96f4>] (pcie_port_device_register+0x1c8/0x2a8)
[<802c96f4>] (pcie_port_device_register) from [<802c9a6c>] (pcie_portdrv_probe+0x3c/0xa4)
[<802c9a6c>] (pcie_portdrv_probe) from [<802bf8e8>] (pci_device_probe+0x74/0xc8)
[<802bf8e8>] (pci_device_probe) from [<8034c778>] (driver_probe_device+0x110/0x24c)
[<8034c778>] (driver_probe_device) from [<8034ad7c>] (bus_for_each_drv+0x64/0x98)
[<8034ad7c>] (bus_for_each_drv) from [<8034c638>] (device_attach+0x74/0x88)
[<8034c638>] (device_attach) from [<802b7dac>] (pci_bus_add_device+0x34/0x64)
[<802b7dac>] (pci_bus_add_device) from [<802b7ec4>] (pci_bus_add_devices+0x3c/0xa0)
[<802b7ec4>] (pci_bus_add_devices) from [<800137ec>] (pci_common_init_dev+0x224/0x2ec)
[<800137ec>] (pci_common_init_dev) from [<80caafd8>] (dw_pcie_host_init+0x640/0x670)
[<80caafd8>] (dw_pcie_host_init) from [<80cab300>] (imx6_pcie_probe+0x2e4/0x328)
[<80cab300>] (imx6_pcie_probe) from [<8034def0>] (platform_drv_probe+0x44/0xa4)
[<8034def0>] (platform_drv_probe) from [<8034c778>] (driver_probe_device+0x110/0x24c)
[<8034c778>] (driver_probe_device) from [<8034c984>] (__driver_attach+0x8c/0x90)
[<8034c984>] (__driver_attach) from [<8034acd0>] (bus_for_each_dev+0x6c/0xa0)
[<8034acd0>] (bus_for_each_dev) from [<8034bf30>] (bus_add_driver+0x148/0x1f0)
[<8034bf30>] (bus_add_driver) from [<8034cf80>] (driver_register+0x78/0xf8)
[<8034cf80>] (driver_register) from [<8034df78>] (platform_driver_probe+0x20/0xa8)
[<8034df78>] (platform_driver_probe) from [<8000889c>] (do_one_initcall+0xf8/0x154)
[<8000889c>] (do_one_initcall) from [<80c80c54>] (kernel_init_freeable+0x138/0x1d8)
[<80c80c54>] (kernel_init_freeable) from [<8067b888>] (kernel_init+0x8/0xe8)
[<8067b888>] (kernel_init) from [<8000e538>] (ret_from_fork+0x14/0x3c)
---[ end trace c3533c29af9b31ae ]---
pcie_pme: probe of 0000:00:00.0:pcie01 failed with error -22
...
...
PCI: enabling device 0000:01:00.0 (0140 -> 0143)
rtl8188ee: Using firmware rtlwifi/rtl8188efw.bin
------------[ cut here ]------------
rtlwifi: wireless switch is on
WARNING: CPU: 0 PID: 184 at kernel/irq/manage.c:1412 request_threaded_irq+0xfc/0x124()
Modules linked in: rtl8188ee(+) rtl_pci rtlwifi mac80211 cfg80211 evbug
CPU: 0 PID: 184 Comm: udevd Tainted: G W 3.14.28-svn1420 #1
[<80015638>] (unwind_backtrace) from [<80011714>] (show_stack+0x10/0x14)
[<80011714>] (show_stack) from [<806801a8>] (dump_stack+0x7c/0xbc)
[<806801a8>] (dump_stack) from [<8002d9a8>] (warn_slowpath_common+0x70/0x8c)
[<8002d9a8>] (warn_slowpath_common) from [<8002da60>] (warn_slowpath_null+0x1c/0x24)
[<8002da60>] (warn_slowpath_null) from [<80069f94>] (request_threaded_irq+0xfc/0x124)
[<80069f94>] (request_threaded_irq) from [<7f0b4558>] (rtl_pci_probe+0x17b0/0x1a18 [rtl_pci])
[<7f0b4558>] (rtl_pci_probe [rtl_pci]) from [<802bf8e8>] (pci_device_probe+0x74/0xc8)
[<802bf8e8>] (pci_device_probe) from [<8034c778>] (driver_probe_device+0x110/0x24c)
[<8034c778>] (driver_probe_device) from [<8034c984>] (__driver_attach+0x8c/0x90)
[<8034c984>] (__driver_attach) from [<8034acd0>] (bus_for_each_dev+0x6c/0xa0)
[<8034acd0>] (bus_for_each_dev) from [<8034bf30>] (bus_add_driver+0x148/0x1f0)
[<8034bf30>] (bus_add_driver) from [<8034cf80>] (driver_register+0x78/0xf8)
[<8034cf80>] (driver_register) from [<8000889c>] (do_one_initcall+0xf8/0x154)
[<8000889c>] (do_one_initcall) from [<800850c0>] (load_module+0x198c/0x1eb4)
[<800850c0>] (load_module) from [<80085740>] (SyS_finit_module+0x68/0x78)
[<80085740>] (SyS_finit_module) from [<8000e4a0>] (ret_fast_syscall+0x0/0x30)
---[ end trace c3533c29af9b31b0 ]---
rtl8188ee: probe of 0000:01:00.0 failed with error -22
2. I refer following URL, PCIE function can work.
a) Reference URL:
https://community.freescale.com/message/568158#568158
https://community.freescale.com/message/563729#563729
b) Removing the lines for '#address-cells' and '#size-cells' fixed it:
diff --git a/arch/arm/boot/dts/imx6qdl.dtsi b/arch/arm/boot/dts/imx6qdl.dtsi
index 732f2d2..e0cd2b1 100644
--- a/arch/arm/boot/dts/imx6qdl.dtsi
+++ b/arch/arm/boot/dts/imx6qdl.dtsi
@@ -48,8 +48,6 @@
intc: interrupt-controller@00a01000 {
compatible = "arm,cortex-a9-gic";
#interrupt-cells = <3>;
- #address-cells = <1>;
- #size-cells = <1>;
interrupt-controller;
reg = <0x00a01000 0x1000>,
<0x00a00100 0x100>;
3. Will this solution is the right solution?
Thank you.
Best Regards,
Alex Cheng
Hello,
Strictly speaking, interrupts in device tree can be described using the
following properties:
• interrupt-controller
• #interrupt-cells
• interrupt-parent
• interrupts
And #address-cells, #size-cells are not needed here.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------