Hello,
I have implemented an OV5647 camera board which connects to my i.MX6 quad Wandboard. I am having trouble getting images from the driver and need some help figuring out why. I have reviewed about a dozen related threads on this forum, and tried to carefully implement their suggestions.
Here are the steps I have taken so far:
I have to guess that what is going on is that the image format is not being handled correctly, but I can't tell from the tracing.
Some specific questions:
The following is what I get with DEBUG tracing on in the drivers:
[ 1160.505314] End of mxc_v4l2_g_fmt: crop_current widthxheight 1280 x 960
[ 1160.505352] In MVC:mxc_v4l_ioctl
[ 1160.505360] In MVC: mxc_v4l_do_ioctl c0405602
[ 1160.505373] In MVC:mxc_v4l_ioctl
[ 1160.505380] In MVC: mxc_v4l_do_ioctl c0405602
[ 1160.505458] In MVC:mxc_v4l_ioctl
[ 1160.505465] In MVC: mxc_v4l_do_ioctl c0445624
[ 1160.505472] case default or not supported
[ 1160.505528] In MVC:mxc_v4l_ioctl
[ 1160.505535] In MVC: mxc_v4l_do_ioctl c02c563a
[ 1160.505540] case VIDIOC_CROPCAP
[ 1160.505547] In MVC:mxc_v4l_ioctl
[ 1160.505552] In MVC: mxc_v4l_do_ioctl 4014563c
[ 1160.505561] case VIDIOC_S_CROP
[ 1160.505567] Cropping Input to ipu size 1280 x 960
[ 1160.505678] In MVC:mxc_v4l_ioctl
[ 1160.505686] In MVC: mxc_v4l_do_ioctl c0145608
[ 1160.505693] case VIDIOC_REQBUFS
[ 1160.505697] In MVC:mxc_streamoff
[ 1160.505702] MVC: In mxc_free_frame_buf
[ 1160.505709] In MVC:mxc_allocate_frame_buf - size=152064
[ 1160.508739] In MVC:mxc_v4l_ioctl
[ 1160.508746] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508752] case VIDIOC_QUERYBUF
[ 1160.508759] In MVC:mxc_v4l2_buffer_status
[ 1160.508904] In MVC:mxc_mmap
[ 1160.508911] pgoff=0x184c0, start=0x45dbd000, end=0x45de3000
[ 1160.508933] In MVC:mxc_v4l_ioctl
[ 1160.508939] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508944] case VIDIOC_QUERYBUF
[ 1160.508949] In MVC:mxc_v4l2_buffer_status
[ 1160.508966] In MVC:mxc_mmap
[ 1160.508972] pgoff=0x18300, start=0x46549000, end=0x4656f000
[ 1160.508987] In MVC:mxc_v4l_ioctl
[ 1160.508992] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.508997] case VIDIOC_QUERYBUF
[ 1160.509002] In MVC:mxc_v4l2_buffer_status
[ 1160.509013] In MVC:mxc_mmap
[ 1160.509019] pgoff=0x18340, start=0x46700000, end=0x46726000
[ 1160.509033] In MVC:mxc_v4l_ioctl
[ 1160.509039] In MVC: mxc_v4l_do_ioctl c0445609
[ 1160.509044] case VIDIOC_QUERYBUF
[ 1160.509049] In MVC:mxc_v4l2_buffer_status
[ 1160.509058] In MVC:mxc_mmap
[ 1160.509064] pgoff=0x19f00, start=0x467ed000, end=0x46813000
[ 1160.509085] In MVC:mxc_v4l_ioctl
[ 1160.509092] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509097] case VIDIOC_QBUF
[ 1160.509104] In MVC:mxc_v4l_ioctl
[ 1160.509110] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509115] case VIDIOC_QBUF
[ 1160.509121] In MVC:mxc_v4l_ioctl
[ 1160.509126] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509131] case VIDIOC_QBUF
[ 1160.509138] In MVC:mxc_v4l_ioctl
[ 1160.509143] In MVC: mxc_v4l_do_ioctl c044560f
[ 1160.509148] case VIDIOC_QBUF
[ 1160.509154] In MVC:mxc_v4l_ioctl
[ 1160.509160] In MVC: mxc_v4l_do_ioctl 40045612
[ 1160.509166] case VIDIOC_STREAMON
[ 1160.509170] In MVC:mxc_streamon
[ 1160.509175] IPU:In prp_enc_enabling_tasks
[ 1160.509981] In prp_enc_setup
[ 1160.509988] YUV420
[ 1160.510026] eba 184c0000
[ 1160.510033] eba 18300000
[ 1160.510230] In MVC:mxc_poll
[ 1160.510243] In MVC:mxc_v4l_ioctl
[ 1160.510250] In MVC: mxc_v4l_do_ioctl c0445611
[ 1160.510256] case VIDIOC_DQBUF
[ 1160.510261] In MVC:mxc_v4l_dqueue
[ 1170.504999] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 1170.511966] In MVC:mxc_poll
[ 1170.511983] In MVC:mxc_v4l_ioctl
[ 1170.511991] In MVC: mxc_v4l_do_ioctl c0445611
[ 1170.511997] case VIDIOC_DQBUF
[ 1170.512001] In MVC:mxc_v4l_dqueue
[ 1180.504959] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 1180.511757] In MVC:mxc_poll
[ 1180.511773] In MVC:mxc_v4l_ioctl
[ 1180.511783] In MVC: mxc_v4l_do_ioctl c0445611
[ 1180.511789] case VIDIOC_DQBUF
[ 1180.511794] In MVC:mxc_v4l_dqueue
[ 1190.504954] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
Solved! Go to Solution.
[Edit Oct 24 2014: After receiving various messages from other users about what patches we have used, I have attached the relevant patches in a zip file. These contain the MT9M031 driver, OV5647 driver and changes to the freescale kernel to (1) enable Greyscale/Raw capture and (2) allow correctly synch'd capture from a MIPI channel other than channel 0]
I finally got it working a couple of days ago. I had a couple of problems but basically I hit and resolved the following issues:
At this point I am getting Bayer patter data in memory and will soon look into using the graphics coprocessor or IPU to handle demosaicing. When the code is a little cleaner I will also post my kernel patch and driver file.
Hi Dave,
Sub:Ov9712 camera with Imx6 Bayer format support
i have read your threads regarding the Bayer format support for imx6 .I have used imx6 solo processor with ov9712 omni vision camera in parallel port interface .
Ov9712 1MP camera does not have ISP and supports output formats (10-bit) raw RGB data, our camera connection in hardware side sensor->imx6 solo processor 8 bit (CSIO_Data12-CSIO_Data19).How can i achieve this conversion from camera RGB bayer datas output to YUV422 format .IPU does not support the bayer format so i need to convert bayer data to YUV422 data before giving this data to IPU unit.
Please suggest your ideas how to access this bayer data format in imx6 solo processor.
Thanks by,
Venkat
Thanks Dave,
I can now see data flowing through the pipeline in the GREY mode. Although I don't think I am even close yet in having the data through correctly. And the behaviour is not very consistent with respect to the different capturing test applications I used (gstreamer, v4l2 capture example, Freescale v4l2 unit tests). But clearly I am making big progress here now. Thanks again!
-Timo
More info (I've managed to enable some IPU tracing):
[ 264.365866] imx-ipuv3 imx-ipuv3.0: CSI_SENS_CONF = 0x00001B00
[ 264.365875] imx-ipuv3 imx-ipuv3.0: CSI_ACT_FRM_SIZE = 0x03BF04FF
[ 265.948470] Grey/Generic
[ 265.948485] imx-ipuv3 imx-ipuv3.0: init channel = 19
[ 265.948508] imx-ipuv3 imx-ipuv3.0: resizing from 960 -> 960 pixels, downsize=0, resize=1.0 (reg=8192)
[ 265.948527] imx-ipuv3 imx-ipuv3.0: initializing idma ch 20 @ ea8c0500
[ 265.948550] imx-ipuv3 imx-ipuv3.0: ch 20 word 0 - 00000000 00000000 00000000 E0002800 000EFC9F
[ 265.948563] imx-ipuv3 imx-ipuv3.0: ch 20 word 1 - 02D80000 005B0000 20C3C000 00027FC0 00000000
[ 265.948573] imx-ipuv3 imx-ipuv3.0: PFS 0x6,
[ 265.948582] imx-ipuv3 imx-ipuv3.0: BPP 0x5,
[ 265.948591] imx-ipuv3 imx-ipuv3.0: NPB 0xf
[ 265.948598] imx-ipuv3 imx-ipuv3.0: FW 1279,
[ 265.948606] imx-ipuv3 imx-ipuv3.0: FH 959,
[ 265.948614] imx-ipuv3 imx-ipuv3.0: EBA0 0x16c00000
[ 265.948622] imx-ipuv3 imx-ipuv3.0: EBA1 0x16c00000
[ 265.948631] imx-ipuv3 imx-ipuv3.0: Stride 2559
[ 265.948638] imx-ipuv3 imx-ipuv3.0: scan_order 0
[ 265.948646] imx-ipuv3 imx-ipuv3.0: uv_stride 0
[ 265.948656] imx-ipuv3 imx-ipuv3.0: u_offset 0x0
[ 265.948664] imx-ipuv3 imx-ipuv3.0: v_offset 0x0
[ 265.948672] imx-ipuv3 imx-ipuv3.0: Width0 0+1,
[ 265.948679] imx-ipuv3 imx-ipuv3.0: Width1 0+1,
[ 265.948688] imx-ipuv3 imx-ipuv3.0: Width2 0+1,
[ 265.948695] imx-ipuv3 imx-ipuv3.0: Width3 0+1,
[ 265.948703] imx-ipuv3 imx-ipuv3.0: Offset0 0,
[ 265.948712] imx-ipuv3 imx-ipuv3.0: Offset1 0,
[ 265.948720] imx-ipuv3 imx-ipuv3.0: Offset2 0,
[ 265.948727] imx-ipuv3 imx-ipuv3.0: Offset3 0
[ 265.948741] eba 18c00000
[ 265.948749] eba 16000000
[ 265.948756] Calling enc_enable_csi
[ 265.948763] Enabling ipu 0 with csi 0
[ 265.949043] In MVC:mxc_poll
[ 265.949063] In MVC:mxc_v4l_ioctl
[ 265.949072] In MVC: mxc_v4l_do_ioctl c0445611
[ 265.949080] case VIDIOC_DQBUF
[ 265.949084] In MVC:mxc_v4l_dqueue
[ 275.947279] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 275.955480] In MVC:mxc_poll
[ 275.955501] In MVC:mxc_v4l_ioctl
[ 275.955510] In MVC: mxc_v4l_do_ioctl c0445611
[ 275.955516] case VIDIOC_DQBUF
[ 275.955520] In MVC:mxc_v4l_dqueue
[ 285.955111] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
[ 780.248845] IPU_CONF = | 0x100006A4 |
[ 780.248850] IDMAC_CONF = | 0x0000002F |
[ 780.248856] IDMAC_CHA_EN1 = | 0x00900000 |
[ 780.248862] IDMAC_CHA_EN2 = | 0x00000000 |
[ 780.248868] IDMAC_CHA_PRI1 = | 0x18800001 |
[ 780.248875] IDMAC_CHA_PRI2 = | 0x00000000 |
[ 780.248880] IDMAC_BAND_EN1 = | 0x00000000 |
[ 780.248886] IDMAC_BAND_EN2 = | 0x00000000 |
[ 780.248893] IPU_CHA_DB_MODE_SEL0 = | 0x00100000 |
[ 780.248899] IPU_CHA_DB_MODE_SEL1 = | 0x00000000 |
[ 780.248906] IPU_CHA_TRB_MODE_SEL0 = | 0x00800000 |
[ 780.248913] IPU_CHA_TRB_MODE_SEL1 = | 0x00000000 |
[ 780.248919] DMFC_WR_CHAN = | 0x00000090 |
[ 780.248925] DMFC_WR_CHAN_DEF = | 0x202020F6 |
[ 780.248931] DMFC_DP_CHAN = | 0x000096CA |
[ 780.248937] DMFC_DP_CHAN_DEF = | 0x2020F6F6 |
[ 780.248943] DMFC_IC_CTRL = | 0x00000002 |
[ 780.248949] IPU_FS_PROC_FLOW1 = | 0x00000000 |
[ 780.248954] IPU_FS_PROC_FLOW2 = | 0x00000000 |
[ 780.248961] IPU_FS_PROC_FLOW3 = | 0x00000000 |
[ 780.248967] IPU_FS_DISP_FLOW1 = | 0x00000000 |
[ 780.248973] IPU_VDIC_VDI_FSIZE = | 0x00000000 |
[ 780.248978] IPU_VDIC_VDI_C = | 0x00000000 |
[ 780.248984] IPU_IC_CONF = | 0x00000001 |
This tells me that (1) I am setting the format and size for the IPU registers correctly (Step A) 4. in the "Some Experience when enabling MIPI.." guide.
Still no frames, and no error message telling me what is failing.
There is one more clue however. I can only attempt to capture once from the device. The second time I capture, I get the following error and have to reboot to start capturing again:
[ 440.222233] IPU:In prp_enc_enabling_tasks
[ 440.230557] imx-ipuv3 imx-ipuv3.0: handler already installed on irq 20
This suggests that the IPU is the problem, and that it is not getting cleaned up properly.
Can anyone tell me how to dump CPU registers from the command line, in order to inspect the state of all these registers? Or is that just something I have to code into (or enable) in the kernel?
I can now get frames (although not actually correct width/height, etc), with a little bit of acrobatics:
When it is working, I get "Warning IPU_INT_STAT_5 = 1", which seems to mean that the EOF interrupt is already set. This would make sense since I am now getting frames with incorrect vertical sync (chopped images).
Once again, if anyone with knowledge of the IPU and Bayer / Generic capture can comment, I would be most grateful! I am more than a little surprised at the lack of support from Freescale on this, especially given that I intend to share both my driver and tips on supporting Bayer and Generic capture.
Thanks Jimmy.
Have just read through the chapter and I don't see any significant mention of the MIPI interface. Don't I need to make sure the MIPI capture is working?
This guide would have been very helpful to me as I was implementing the driver. I had to figure out And guess at a bunch of things that it explains.
Do you have any thoughts on what would lead to the MIPI PHY having correct state and no errors, but no images coming through?
Dave
More information here :
Yes, I have reviewed that in detail, verifying register settings all the way through. It doesn't help with figuring out why I am not getting frame interrupts. From what I can tell it could be any of the following:
1. Incorrectly configured CSI2IPU gasket
2. Bayer image format not supported, or special magic needed to get it copied into memory (there are many threads on this topic and I have reviewed them all carefully.
3. MIPI connection not working correctly (seems not to be the issue since error registers are clear and state is 0x300)
4. Camera not correctly configured
It would be very helpful to have some feedback on which of these are likely to be problematic, based on the dmesg trace above.
One thing: even though the MIPI PHY state is 0x300, I have not been able to see any data on my scope, and there are high levels of noise throughout the wandboard system. Could it be that the PHY state is okay, but in fact the camera is not sending any data? Also, I never see the PHY state change to 0x330, which I would expect if either of the data lanes goes into stop mode.