i.MX6 NOR Flash questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 NOR Flash questions

549 Views
ramansubramania
Contributor I

The imx6 can read spi
nor to boot. Is there support to write spi nor?

Customer would like spi NOR to store two
runtime images, and in a crash want to dump core to it.

Can this done?

Labels (1)
0 Kudos
Reply
1 Reply

419 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raman

spi nor can be written in uboot or linux.

However when system crashes, usually it can be recovered only

with reboot using wdog or other methods. That is in crash situation

it would not be able to make sensible/reliable dump operations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply