: i.MX6 LTIB installation, can't find download link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

: i.MX6 LTIB installation, can't find download link

1,408 Views
frankchenmh
Contributor III

Hi,

The link is not available now. But I need this BSP for some reasons. Could anyone let me know where to download the old release? Thanks!

Regards,

Frank

0 Kudos
Reply
5 Replies

1,249 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I 've sent You message via e-mail.

Regards,

Yuri.

1,171 Views
TKayO
Contributor III

Dear @Yuri 

 

Can you help me with the same information?

 

I also need legacy BSP for my own reason.

 

Regards,

1,167 Views
Yuri
NXP Employee
NXP Employee

@TKayO 
Hello,

  what NXP Linux BSP release do You mean?

You can create request:

https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu

Regards,
Yuri.

1,164 Views
TKayO
Contributor III

Dear @Yuri 

I need gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 toolchain

and from some other post, you mentioned 

"L3.0.35_4.1.0_130816_source.tar.gz" BSP contains it.

Thank you.

0 Kudos
Reply

1,249 Views
frankchenmh
Contributor III

Hi Yuri,

Thanks a lot for your help! I will download it from the google disk.

Regards,

Frank

发件人: Yuri

发送时间: 2018年10月29日 17:52

收件人: Frank Chen

主题: Re: - Re: : i.MX6 LTIB installation, can't find download link

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: : i.MX6 LTIB installation, can't find download link

reply from Yuri Muhin <https://community.nxp.com/people/Yuri?et=watches.email.thread> in i.MX Processors - View the full discussion <https://community.nxp.com/message/1073816?commentID=1073816&et=watches.email.thread#comment-1073816>

0 Kudos
Reply